Arduino
  • Products
  • More
Arduino
Arduino Forum Starting with Arduino Uno or Chipkit Uno32?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 419 subscribers
  • Views 1391 views
  • Users 0 members are here
  • chipkit
  • arduino
Related

Starting with Arduino Uno or Chipkit Uno32?

e14 Contributor
e14 Contributor over 14 years ago

Hi there,

 

I was about to buy my first arduino device, a arduino uno. But seeing the chipkit uno32 at roughly the same price, is it worth starting with the classic one? My first apps will not need high speed but who knows for future.

 

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • fustini
    fustini over 14 years ago +1
    The Digilent ChipKit Uno32 ChipKit Uno32 along with the ChipKit Max32 are very interesting as they are the only non-AVR boards that I know which are software compatible with the Arduino platform. Their…
  • YT2095
    YT2095 over 14 years ago in reply to e14 Contributor +1
    after I got a little jaded with the "shieds" I bought a small bread board and made my own breadboard "shield" for it with vero board and a few SIL headers, this is also good for small projects and quite…
  • fustini
    fustini over 14 years ago in reply to ntewinkel +1
    Hi - I've not used the Amicus but from what I know it is just hardware compatible and offers it's own BASIC environment. The ARM-based Maple from LeafLabs is another example of a board that is hardware…
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    You are right, I will stay with well documented and well known by the community for now. By the way I will not go bankrupt if I need to buy something different later.

    As for the shield I did not think a lot about it. I was thinking about getting one proto shield, maybe it would be smarter to prefer a large breadboard.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    You are right, I will stay with well documented and well known by the community for now. By the way I will not go bankrupt if I need to buy something different later.

    As for the shield I did not think a lot about it. I was thinking about getting one proto shield, maybe it would be smarter to prefer a large breadboard.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • YT2095
    YT2095 over 14 years ago in reply to e14 Contributor

    after I got a little jaded with the "shieds" I bought a small bread board and made my own breadboard "shield" for it with vero board and a few SIL headers, this is also good for small projects and quite cheap when compared to the solder type proto-shields that you can really only use once.

    but for Long term, get a Large breadboard and a Nano, this will not only assist in Arduino based prototyping, but also the arduino can be made into almost anything for prototyping Other chips image

     

    anything from a simple binary counter or serial I/O to a frequency or random number generator etc...

     

    you can also make simple plug in modules such as a bank of 8 LEDs with resistors, or a bank of DIP switches, or a seven segment display etc... all these will save time when building on breadboard and are perfectly transportable to other projects.

    that way you only ever have to do the donkey work once image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 14 years ago in reply to YT2095

    I agree with YT2095 - I also have an Arduino Nano set up in a (relatively big) breadboard, and it works easily and conveniently with anything from bare parts (LEDs, switches, logic chips) to boards (like Bluetooth, distance finders, displays). LCD displays, for example just plug into the breadboard underneath it. Then just hook it all up with m-m patch cords.

     

    Plus it can provide any other project you do with 5v or 3.3v from the Nano image

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago in reply to e14 Contributor

    I really like Arduino holders which have space to stick a breadboard.  I use these for most prototyping and have only used a protoshield a couple times when I wanted to semi-finalize a design.

     

    I own and recommend these Adafruit and Sparkfun holders:

     

    http://www.sparkfun.com/products/10059

    http://www.adafruit.com/products/275

     

    I also own this holder which I use for my Arduino Mega:

     

    http://store.tautic.com/acrylic-prototyping-board-for-chipkit-small.html