Arduino Forum Using a Pcduino with camera.
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
  • Replies 6 replies
  • Subscribers 401 subscribers
  • Views 509 views
  • Users 0 members are here
  • ov7670
  • pcduino
Related

Using a Pcduino with camera.

clem57
clem57 over 9 years ago

I am going to order a camera for Pcduino to program.

Clem

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 9 years ago in reply to clem57 +1
    Perhaps take a look at the Vimicro VC0706 camera which outputs compressed over serial. tutorials:products:camera:index.html [AdaWiki]
Parents
  • clem57
    clem57 over 9 years ago

    OV7670  is this a good one?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 9 years ago in reply to clem57

    Hi Clem!

     

    Raw camera modules like OV7670 just spit out a stream of data at a high speed, and it is up to the user program to capture it at the right HSYNC and VSYNC points in time. It is uncompressed, raw data. Also a fair amount of memory is needed, i.e. number of pixels in X direction times Y direction, so about 300kbytes for a 640x480 frame with 8 bits per pixel, which is only 256 colors, so in practice you want 16 or 24 bits per pixel.

    However, the instructables page shows some camera module with RX and TX pins only. So it seems to be some module with on-board processor which captures the stream of data into memory on the module, and makes it available over a UART, perhaps compressed (e.g. JPEG frames like a camera, so less memory is needed). But OV7670 is a part number for a raw camera module, so they have forgotten to mention the actual module.

    Their module should be fine if your requirement is to capture individual frames, but without knowing which module they mean, it is not possible to tell if it is suitable.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 9 years ago in reply to shabaz

    Ugh. Tricky if you need to process this much data and not store away.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 9 years ago in reply to clem57

    Perhaps take a look at the Vimicro VC0706 camera which outputs compressed over serial.

    tutorials:products:camera:index.html [AdaWiki]

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 9 years ago in reply to beacon_dave

    I have to check that out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 9 years ago in reply to clem57

    Are you able to run OpenCV on the pcDuino ?

     

    If so you should be able to use any UVC compliant USB webcam as a camera source.

    ( UVC compliant camera list at: Linux UVC driver & tools )

     

    If you have access to an Intel Galileo then there is a whole chapter on using USB web cameras with OpenCV in Manoel Carlos Ramon's book "Intel Galileo and Intel Galileo Gen 2: API Features and Arduino Projects for Linux Programmers"

    ( It's an 'open access' book so you can take a read here:

    Using OpenCV - Springer )

     

    It covers image and video capture along with image processing such as edge detection, face and eyes detection and so on. You may be able to apply these techniques on the pcDuino platform as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • beacon_dave
    beacon_dave over 9 years ago in reply to clem57

    Are you able to run OpenCV on the pcDuino ?

     

    If so you should be able to use any UVC compliant USB webcam as a camera source.

    ( UVC compliant camera list at: Linux UVC driver & tools )

     

    If you have access to an Intel Galileo then there is a whole chapter on using USB web cameras with OpenCV in Manoel Carlos Ramon's book "Intel Galileo and Intel Galileo Gen 2: API Features and Arduino Projects for Linux Programmers"

    ( It's an 'open access' book so you can take a read here:

    Using OpenCV - Springer )

     

    It covers image and video capture along with image processing such as edge detection, face and eyes detection and so on. You may be able to apply these techniques on the pcDuino platform as well.