Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Tattoo machine controller?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 418 subscribers
  • Views 5347 views
  • Users 0 members are here
Related

Tattoo machine controller?

e14 Contributor
e14 Contributor over 14 years ago

Is it possible to create a tattoo machine controller with arduino?  Tattoo machines usually work between 5-13vdc at less than 1 amp.  Right now most machines operate by opening and closing a circuit containing two electromagnets to pull the armature bar down (pushing the needle down) then breaking the circuit, releasing the needle/bar.

 

I'd be interested in creating something to either draw it's current from a deep cycle marine 12v allowing me to adjust the voltage or more preferably, something that would allow me to take either 120vac or 12vdc and convert it to an appropriate voltage that would allow me to turn on and off the electromagnetic coils using the arduino.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor +1
    After some thinking last night i thought of a way to make the machine more digital. An arduino is along the right line of thinking but isn't powerful enough for the job. What you will want to do is rewire…
  • YT2095
    YT2095 over 14 years ago +1
    personally I`m not entirely certain why you would need an arduino for this at all? if I wanted such a machine, I would use (as stated above) an LM317 feeding the base of a 2n3055 transistor giving you…
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to billabott +1
    Google translate doesn't do Geek > Noob yet...
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    The tattoo machine is a very simple machine and works quite well. When something so simple works so well there is no point it messing things up and trying to over complicate it. The machine handles the firing of the coils just fine without a computer helping it along. As you probably know, when you turn the power on to the machine the coils fire drawing the armature bar to them and driving the needle to the skin. As soon as that happens the front spring leaves the adjustment screw breaking the circuit to the coils allowing the rear spring the draw the Armature bar back up making contact with the adjustment screw again and firing the coils again. A combination of the voltage from the power supply and the adjustment screw controls how smooth and how fast the machine runs. So where would an arduino be of any help? If you want to use it to control the voltage there are much simpler circuits you can make using an LM317M adjustable voltage regulator. If you wanted to make give it a digital readout an Arduino could come in handy for that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    The tattoo machine is a very simple machine and works quite well. When something so simple works so well there is no point it messing things up and trying to over complicate it. The machine handles the firing of the coils just fine without a computer helping it along. As you probably know, when you turn the power on to the machine the coils fire drawing the armature bar to them and driving the needle to the skin. As soon as that happens the front spring leaves the adjustment screw breaking the circuit to the coils allowing the rear spring the draw the Armature bar back up making contact with the adjustment screw again and firing the coils again. A combination of the voltage from the power supply and the adjustment screw controls how smooth and how fast the machine runs. So where would an arduino be of any help? If you want to use it to control the voltage there are much simpler circuits you can make using an LM317M adjustable voltage regulator. If you wanted to make give it a digital readout an Arduino could come in handy for that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    I don't know if I want to improve it but I'd like to change how it works.  I know it's efficient but there are companies out there now offering systems that basically let you modify the force and duration of the needle strike electronically, the set screw only modifies the length of travel for the needle.

     

    either way, I'd really like running my machine on a 12v DC battery.  Could I just use a pot for that ?

     

    ^^^ pretty new to electronics, just got my first arduino a few days ago and the ideas are flying image    

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    No a pot on its own won't be enoug. You will need the LM317M and a few other components to create a circuit that can regulat the output of the battery. Here is a simple circuit that will do it for you.

    http://www.circuit-innovations.co.uk/LM317.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • billabott
    billabott over 14 years ago in reply to e14 Contributor

    Chad Kovac wrote:

     

    ... modify the force and duration of the needle strike electronically, the set screw only modifies the length of travel for the needle.

     

    Isn't that something the artist controls with his/her eyes and using tactile feedback in his/her hand?

    Would you care to provide a link to where these new machine types specifications are documented?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    After some thinking last night i thought of a way to make the machine more digital. An arduino is along the right line of thinking but isn't powerful enough for the job.

     

    What you will want to do is rewire the tattoo machine so the power goes directly to the coils and not through the adjustment screw. You will need an adjustable Puls Width Modulator circuit that can handle up to 12V and you need and adjustable power supply to vary the voltage. The PWM circuit will modulate the DC voltage on and off at an adjustable rate. So you will have control of the voltage and the frequency the machine operates at. The trick will be getting the PWM to modulate slow enough so the coils are able to do there job. If the modulation is too fast it will be like the power is constantly on them and the coils could burn out.