Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Tattoo machine controller?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 418 subscribers
  • Views 5347 views
  • Users 0 members are here
Related

Tattoo machine controller?

e14 Contributor
e14 Contributor over 14 years ago

Is it possible to create a tattoo machine controller with arduino?  Tattoo machines usually work between 5-13vdc at less than 1 amp.  Right now most machines operate by opening and closing a circuit containing two electromagnets to pull the armature bar down (pushing the needle down) then breaking the circuit, releasing the needle/bar.

 

I'd be interested in creating something to either draw it's current from a deep cycle marine 12v allowing me to adjust the voltage or more preferably, something that would allow me to take either 120vac or 12vdc and convert it to an appropriate voltage that would allow me to turn on and off the electromagnetic coils using the arduino.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor +1
    After some thinking last night i thought of a way to make the machine more digital. An arduino is along the right line of thinking but isn't powerful enough for the job. What you will want to do is rewire…
  • YT2095
    YT2095 over 14 years ago +1
    personally I`m not entirely certain why you would need an arduino for this at all? if I wanted such a machine, I would use (as stated above) an LM317 feeding the base of a 2n3055 transistor giving you…
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to billabott +1
    Google translate doesn't do Geek > Noob yet...
Parents
  • YT2095
    YT2095 over 14 years ago

    personally I`m not entirely certain why you would need an arduino for this at all?

    if I wanted such a machine, I would use (as stated above) an LM317 feeding the base of a 2n3055 transistor giving you variable voltage with plenty of room for current, and then have a second 2n3055 gate, triggered by a simple 555 chip.

    that would give you a variable voltage and frequency PSU also.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to YT2095

    This  type device will give more control of Force(duty cycle) and Speed(frequency). The stroke adjustment remains mechanical. Is Volt and Hz control w (2) pots? Can you draw this schematic..or point me to a link.

    thanks for any help

     

    Unimax sells 'Tattinator'

    Infinity also has an interesting control.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to YT2095

    This  type device will give more control of Force(duty cycle) and Speed(frequency). The stroke adjustment remains mechanical. Is Volt and Hz control w (2) pots? Can you draw this schematic..or point me to a link.

    thanks for any help

     

    Unimax sells 'Tattinator'

    Infinity also has an interesting control.