Arduino
  • Products
  • More
Arduino
Arduino Forum Error in sketch code
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 38 replies
  • Subscribers 418 subscribers
  • Views 4922 views
  • Users 0 members are here
Related

Error in sketch code

e14 Contributor
e14 Contributor over 13 years ago

I am trying to learn to write some code for my BCD clock project.  Before doing the actual clock code I wired up 7 LEDs on my breadboard with 7 resistors.

Then I ran wires from each LED to a digital pin on the Arduino UNO. Specifically pins 7 to 13.

 

Then I wrote some code and tried to upload it but it is flagging 3 errors and I can't see where it is wrong. Probably something that I am missing as a newbie. The errors are as follows:

 

BoardTest:57: error: expected `;' before '{' token

BoardTest:64: error: expected `;' before '{' token

BoardTest:68: error: expected `;' before '{' token

 

The code is as follows:

 

 

// Short sketch to see if breadboard and UNO is properly wired.

 

int led1=7;

int led2=8;

int led3=9;

int led4=10;

int led5=11;

int led6=12;

int led7=13;

 

int seconds=0

 

void setup(){

  ledMode(led1, OUTPUT);

  ledMode(led2, OUTPUT);

  ledMode(led3, OUTPUT);

  ledMode(led4, OUTPUT);

  ledMode(led5, OUTPUT);

  ledMode(led6, OUTPUT);

  ledMode(led7 OUTPUT);

}

 

void loop(){

  seconds++;

    If(seconds == 1){

      digitalWrite(led1, HIGH);

      delay(1000);

    }

    If(seconds == 2){

      digitalWrite(led2, HIGH);

      digitalWrite(led1, LOW);

      delay(1000);

    }

  If(seconds == 3){

      digitalWrite(led1, HIGH);

      delay(1000);

    }

    If(seconds == 4){

      digitalWrite(led3, HIGH);

      digitalWrite(led2, LOW);

      digitalWrite(led1, LOW);

      delay(1000);

    }

    If(seconds == 5){

      digitalWrite(led1, HIGH);

      delay(1000);

    }

    If(seconds == 6){

      digitalWrite(led2, HIGH);

      digitalWrite(led1, LOW);

      delay(1000);

    }

    If(seconds == 7){

      digitalWrite(led1, HIGH);

      delay(1000);

    }

    If(seconds == 8){

      digitalWrite(led4, HIGH);

      digitalWrite(led3, LOW);

      digitalWrite(led2, LOW);

      digitalWrite(led1, LOW);

      delay(1000);

    }

    If(seconds == 9){

      digitalWrite(led1, HIGH);

      delay(1000);

    }

    If(seconds == 10){

      digitalWrite(led2, HIGH);

      digitalWrite(led1, LOW);

      delay(1000);

      digitalWrite(led1, LOW);

      digitalWrite(led2, LOW);

      digitalWrite(led3, LOW);

      digitalWrite(led4, LOW);

  seconds=0;

    }

}

 

 

 

Any help appreciated.

 

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago +1
    John, Are those the only errors you're seeing? It looks to me that on line 11, you are missing a semicolon at the end of the line: int seconds=0 and on line 20, you are missing a comma after led7 ledMode…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor +1
    John, A table is just a fancy name for array, although in some languages it might be a fancy type of array such as an associative array. If you have 10 digits, each involving 4 led settings, you might…
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    John,

      Are those the only errors you're seeing?

    It looks to me that on line 11, you are missing a semicolon

    at the end of the line:

       int seconds=0

     

    and on line 20, you are missing a comma after led7

        ledMode(led7 OUTPUT);

     

    and all your "if" statements should use lowercase "if"

    instead of "If".

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    John,

      Are those the only errors you're seeing?

    It looks to me that on line 11, you are missing a semicolon

    at the end of the line:

       int seconds=0

     

    and on line 20, you are missing a comma after led7

        ledMode(led7 OUTPUT);

     

    and all your "if" statements should use lowercase "if"

    instead of "If".

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Yes Coder27, you are correct.  I didn't notice the other errors because they had scrolled up and were not visible.

    This is my first attempt using the Arduino IDE and coding in 'C'.

     

    I have added the semi colon after 'seconds=0' and the comma after the (led7, OUTPUT).  As well I have changed all of the If to if.

     

    Thanks for pointing these out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • billabott
    billabott over 13 years ago in reply to e14 Contributor

    One thing you seem to have overlooked JohnC.

    That tiny little number in the lowest left hand corner of the IDE is the line number of the .pde being edited.  Moving the cursor to a different line changes the number.  Good for seeking out the location the error message pertains to.  Don't you agree?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to billabott

    I think the problem here is that the error message indicating a missing

    semicolon was misleading.  The problem was a mis-capitalized keyword,

    rather than a missing semicolon.  It didn't help that previous error messages

    had scrolled off the screen, since that might lead one to believe that the

    previous if-statements were OK.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • billabott
    billabott over 13 years ago in reply to e14 Contributor

    http://ecx.images-amazon.com/images/I/41w7lABe%2B%2BL._SL500_AA300_.jpg

    Merry Kiss-a-Gir.