Arduino
  • Products
  • More
Arduino
Arduino Forum Digital Thermometer Project.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 416 subscribers
  • Views 262 views
  • Users 0 members are here
Related

Digital Thermometer Project.

e14 Contributor
e14 Contributor over 13 years ago

I am building a simple Digital Thermometer. This is not strictly an Arduino project, I use Arduino to program 2 ATtiny84 that will run the 3-digit, 7-segment LCD.

 

My problem is two fold. First I'm not sure how to direct the current through the LCD: ground to common, or VCC to common. (will ATtiny provide enough power?). If VCC to common how do I program the pins - LOW to display or still HIGH.

 

Second problem is that the LCD fades after a while even it the current is still running through the port. Do I need to multiplex the display?

 

Thanks.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    Hello,

     

    About the current direction it depends on the specification of your LCD. Cathode common type is connected to ground and so anode common type to Vcc.

     

    If it's a common cathode type then the pin should be programmed HIGH to display etc....

     

    In concern of the fade problem i'm not sure that it can be solved by a multiplex circuit as the main problem is about current sinking from the LCD

    and that the tiny pin could not provide it. Try it with a transistor connected to those common cathode or anode it should be much easier !?

     

    Good luck.