Arduino Forum How to do : pin1 + pin2 = Keyboard.press()
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
  • Replies 3 replies
  • Subscribers 401 subscribers
  • Views 230 views
  • Users 0 members are here
Related

How to do : pin1 + pin2 = Keyboard.press()

Former Member
Former Member over 12 years ago

Hello.
Can anyone help me?

I have 32 buttons on 12 wires. It's done like this way: Button 1 is connected to wire1 and wire5. Button 2 is connected to wire1 and wire 5 etc...

Here is list of buttons and wires connected to buttons.

1 - 1;5

2 - 1;6

3 - 1;7

4 - 1;8

5 - 1;9

6 - 1;10

7 - 1;11

8 - 1;12

9 - 2;5

10 - 2;6

11 - 2;7

12 - 2;8

13 - 2;9

14 - 2;10

15 - 2;11

16 - 2;12

17 - 3;5

18 - 3;6

19 - 3;7

20 - 3;8

21 - 3;9

22 - 3;10

23 - 3;11

24 - 3;12

25 - 4;5

26 - 4;6

27 - 4;7

28 - 4;8

29 - 4;9

30 - 4;10

31 - 4;11

32 - 4;12

 

So I need connect these wires to arduino digital pins and I don't know how to program it. I need to do a Keyboard.press() function when is joined pin 1 and 5 etc.. Is there any solution of this?

Thank you in advance for your advice and answers.

Excuse my English. I'm from Czech Republic.

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 12 years ago in reply to ntewinkel +1
    Yeah. This is exactly what I needed. Thank you very much Nico
  • ntewinkel
    ntewinkel over 12 years ago

    I think you'd have to poll the first 4 lines and check for results on the other lines as you do so.

     

    This would be my approach:

    lines 1, 2, 3, 4 are Outputs.

    lines 5 to 12 are Inputs (connected to pulldown resistors)

    start with lines 1-4 set to Low.

     

    loop {

    -for lines 1-4:

    --put the line high, loop through lines 5-12 to see which one is high, and call keyPress() for the key that made it high.

    --return the line to low

    (maybe delay a few milliseconds here)

    }

     

    You would probably want to use a 2D array of characters to easily keep track of which line combinations equal which key was pressed.

     

    edit: you'll also have to keep track of making sure a key press is only called once per physical press!

     

    Good luck!

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 12 years ago in reply to ntewinkel

    Yeah.

    This is exactly what I needed.

    Thank you very much Nico image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 12 years ago in reply to Former Member

    Glad I could help image

     

    I just noticed this library, which I think pretty much does all the hard work for you: http://playground.arduino.cc/Main/KeypadTutorial