Arduino
  • Products
  • More
Arduino
Arduino Forum Butterfly in my Jar
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 415 subscribers
  • Views 321 views
  • Users 0 members are here
Related

Butterfly in my Jar

billabott
billabott over 13 years ago

Has anyone used ATMEL's AVR Butterfly and the free WinAVR?  I was wondering how hard it is to use and what book(s) were found instructive.

 


  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 13 years ago

    I've not used the Butterfly, but I have used (extremely familiar with) AVR devices. Most are programmed in the same manner. Basically, if you have an AVR board, it will likely have a 6-pin or 10-pin DIL header connector, and this is used for programming with a low-cost USB programmer called AVR-ISP mk II (it comes with both the 6-pin and 10-pin mating connector).

    Some of the AVR range have a USB port and can be programmed via USB without the AVR-ISP, using some free software from the Atmel website (this relies on a 'bootloader' on the AVR, but if the bootloader gets erased, I think (not sure) that you'd need the AVR-ISP method to reprogram). The risk of erasing the bootloader is possibly low.

    If you're interested in AVRs, then AVR-ISP is a low-cost, valuable investment - it works with all (or most) of the AVR range.

    Regarding developing for it, it's very easy. WinAVR is highly regarded. Although I like GCC, for AVR I use IAR (they have a free 'kickstart edition' AVR compiler which is code size limited but in practice the code limit is adequate), because their development environment is quite nice.

    I wrote up some steps on how to get started with AVR a while back, maybe it will help (attached).

    Attachments:
    imageprogramming_microcontrollers3.pdf
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 13 years ago

    I've not used the Butterfly, but I have used (extremely familiar with) AVR devices. Most are programmed in the same manner. Basically, if you have an AVR board, it will likely have a 6-pin or 10-pin DIL header connector, and this is used for programming with a low-cost USB programmer called AVR-ISP mk II (it comes with both the 6-pin and 10-pin mating connector).

    Some of the AVR range have a USB port and can be programmed via USB without the AVR-ISP, using some free software from the Atmel website (this relies on a 'bootloader' on the AVR, but if the bootloader gets erased, I think (not sure) that you'd need the AVR-ISP method to reprogram). The risk of erasing the bootloader is possibly low.

    If you're interested in AVRs, then AVR-ISP is a low-cost, valuable investment - it works with all (or most) of the AVR range.

    Regarding developing for it, it's very easy. WinAVR is highly regarded. Although I like GCC, for AVR I use IAR (they have a free 'kickstart edition' AVR compiler which is code size limited but in practice the code limit is adequate), because their development environment is quite nice.

    I wrote up some steps on how to get started with AVR a while back, maybe it will help (attached).

    Attachments:
    imageprogramming_microcontrollers3.pdf