Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino external power
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 418 subscribers
  • Views 1095 views
  • Users 0 members are here
Related

Arduino external power

e14 Contributor
e14 Contributor over 13 years ago

I am working on a sculpture involving multiple servo, dc motor, steppers, and LED's. The power supply is 12v, 8 amp.  I have buck dc to dc converters that work well with the motors but what about powering the board itself?   Do I need a current limiting circuit (LM317) for the Arduino?

 

Keith

  • Sign in to reply
  • Cancel
Parents
  • mcb1
    mcb1 over 13 years ago

    Keith

     

    I explained how to measure the current capabilities of your 'salvaged power supply' in http://www.element14.com/community/message/71204#71204

     

    It might be time to produce the complete wiring diagram and control mechanism to see how you are controlling these motors, etc.

    In the 19 posts about this project I can't recall seeing any specs on the DC motors, but you have gone from using a SN754410NESN754410NE to Mosfets to control them.

     

    You haven't indicated the fuse is blowing that was suggested in http://www.element14.com/community/message/71191#71191

    so there are two possibilities :-

     

    a.     You aren't driving the Mosfets hard enough (hence the heat).

    b.     The salvaged supply is not capable of delivering 8A.

     

    For (a) you can measure the voltage across the mosfet when its turned ON. It should be less than 1v and preferably 0.1v.

    You can also measure the voltage across the motor, and the sum of these should equal 12v (or whatever the supply produces when the motors are ON)

     

    For (b) I have already suggested how you can check the supply in http://www.element14.com/community/message/71204#71204 .

    • So do the three motors run if you connect them straight across the 12v supply.?
    • What voltage is the supply when all three are running.?

     

    Also a (520) mosfet means nothing, there are some other numbers and letters associated with it, although they may not be on it, but you must have a complete part number somewhere.

     

    Does this mean I have grossly underestimated the total current necessary?

     

    Without knowing the total current drawn by the project, how can we answer.?

    What figure did you arrive at when you designed it, and decided to use a 12v 8A (? ) power supply.?

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to mcb1

    Mark,

       Tomorrow I will work on a drawing of the setup. The mosfets were to

    drive three dc motors, at .17 amps, max efficiency, or, 1.2 amps if

    stalled. I will use the SN754410NESN754410NE for the two steppers.

       I may not have been joining all the grounds properly.  Should all three

    grounds (Arduino, 12v, and 6v) be connected?  As explained, the 12v motors

    are running straight from the power supply while the servos are driven from

    the 6v, dc to dc converter. I will draw these details tomorrow after

    replacing the mosfets with a tip31.  The specs state that the Arduino five

    volts is sufficient while the IRF520 Mosfets need 10v to fully open the

    gate.

     

    Keith

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to e14 Contributor

    Keith

    When you do the drawing, I'll be able to comment.

     

     

    Don't go throwing new issues into the problem by replacing FETs with transistors.

     

    Yes the grounds need to be connected....

     

    Also you can't have

    The mosfets were to drive three dc motors,

    and

    As explained, the 12v motors are running straight from the power supply

    It my understanding you have the three DC motors controlled by the mosfet and connected to the 12v supply. (rather than 5 or 6v).

    Your current of 0.17A or 1.2 A stalled is well within the mosfet capabilities.

     

     

    Draw the circuit/connection and I think we will solve your problems....

     

     

    Mark.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to mcb1

    Mark,

       Here is a drawing <http://www.flickr.com/photos/92579016@N08/8554843059/>.

    Sorry, can't do a schematic. Hope this helps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to e14 Contributor

    Keith

     

    Understand you can't do a schematic, but there's detail missing.

    Perhaps you can just draw it and take a photo that is detailed enought (and not blurry) to be able to see it.

    If necessary just include the details of the connections.

     

    It shows a 6v DC-DC converter but you have it fed with 12v, so is it really a 12v to 6v regulator, or is it something truly isolated.?

     

     

    Can you show how the arduino is powered. (is it 12v into the Vin pin??)

    Is the ground from the 12v, 6v converter and Arduino supply connected together.?

     

    You're not showing how you are driving the Mosfet and how the motors connect to them.

    ie does the mosfet switch 12v onto the motor, with the other side of the motor connected to earth, or is one side of the motor connected to 12v, and you're switching the ground.

     

    Have you actually tried any of the other suggestions made in http://www.element14.com/community/message/71639#71639

     

     

    We'll get there, but more detail is required, as in any project.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mcb1
    mcb1 over 13 years ago in reply to e14 Contributor

    Keith

     

    Understand you can't do a schematic, but there's detail missing.

    Perhaps you can just draw it and take a photo that is detailed enought (and not blurry) to be able to see it.

    If necessary just include the details of the connections.

     

    It shows a 6v DC-DC converter but you have it fed with 12v, so is it really a 12v to 6v regulator, or is it something truly isolated.?

     

     

    Can you show how the arduino is powered. (is it 12v into the Vin pin??)

    Is the ground from the 12v, 6v converter and Arduino supply connected together.?

     

    You're not showing how you are driving the Mosfet and how the motors connect to them.

    ie does the mosfet switch 12v onto the motor, with the other side of the motor connected to earth, or is one side of the motor connected to 12v, and you're switching the ground.

     

    Have you actually tried any of the other suggestions made in http://www.element14.com/community/message/71639#71639

     

     

    We'll get there, but more detail is required, as in any project.

     

    Mark