Arduino Forum Help with my simple DIY arduino board so I can put my store bought one away for safe keeping.
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
  • Replies 14 replies
  • Subscribers 405 subscribers
  • Views 1051 views
  • Users 0 members are here
  • hardware
  • led
  • microcontroller
  • uno
  • arduino
  • atmel
Related

Help with my simple DIY arduino board so I can put my store bought one away for safe keeping.

ohiocomputerguy
ohiocomputerguy over 12 years ago

Hi everyone,

I thought it would be cool to make a home made arduino compatible based on the atmega328 so i wouldn't have to worry about " frying" or messing up my store bought arduino when experimenting with something i'm not 100 percent comfortable with.  I've had some problems getting one to work, and i'm not sure if it is my design or maybe just a few bad components, or my lousy soldering skills.  anyhow, i'd appreciat it if someone could take a look at the attached circuit and let me know if you think it should work, or what I need to change.  thanks in advance.

I used fritzing to create the drawing.

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 12 years ago

    Did you check to verify if the Rxd and ~Txd are correctly orientated?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 12 years ago

    Did you check to verify if the Rxd and ~Txd are correctly orientated?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • ohiocomputerguy
    ohiocomputerguy over 12 years ago in reply to Former Member

    yes, connections for data transmission are correct.  My rs232 to usb is marked incorrectly. works perfectly on a breadboard (sometimes the rxd and txd are switched on the cheap chinese rs232 connectors) when my rxd is connected to pin 3 and my txd is connected to pin 2.