Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino Starter Kit?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 418 subscribers
  • Views 1785 views
  • Users 0 members are here
  • arduino
Related

Arduino Starter Kit?

e14 Contributor
e14 Contributor over 13 years ago

Hi, guys. I'm new here. I want to learn something about electronics and Arduino seems to be a nice subject for me. Now I have to purchase the whole kit and wonder which model I should have. It seems that for a starter like me, it's better to use the starter kit. but if i can used the more developed model, like Mega 2560, then I don't have to buy one more in the future when I'm more familiar with it.

 

What do you guys think?

 

Thanks

Manny

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 13 years ago in reply to e14 Contributor +2
    Manny, I have some 23 Arduino's in various formats, and none of them are a Mega. In most cases you only use a few inputs and outputs, so the rest are idle. The basic Arduino has numerous shields that will…
  • billabott
    billabott over 13 years ago in reply to e14 Contributor +1
    Don't forget about adafruit.com. They are very deserving of our support.
  • mcb1
    mcb1 over 13 years ago in reply to billabott +1
    Manny You don't need to purchase a pre-made kit. I ran an introduction course for 8-10yr olds, and I purchased the controller from a local supplier, and the other parts from other sources. The kits were…
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Hi, Manny

    I have just started also and decided to opt for an Arduino Mega 2560 because it has a lot more input and output pins and a greater capacity for sketches than other Arduinos.

    While I expect it will be a while before I utilise the full capacity of the Mega, it is better to have and not need than to need and not have.

     

    I have also just managed to set up my Mega as an ISP for programming ATTiny85 chips and can recommend the Mega although if you are on a tight budget, the Uno is probably good enough.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Aha. It seems that Arduino Mega 2560 is a very popular model. I will consider about it. Thx for your advice.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Aha. It seems that Arduino Mega 2560 is a very popular model. I will consider about it. Thx for your advice.