Arduino
  • Products
  • More
Arduino
Arduino Forum problem recieving sms
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 415 subscribers
  • Views 132 views
  • Users 0 members are here
Related

problem recieving sms

e14 Contributor
e14 Contributor over 13 years ago

Hello good day everyone. I seem to be having some problems. i am using an arduino mega 2560 and connected to it i have a gsm module sm5001-B module. I am able to send text messages but recieving is a bit more tricky. I have the following code below,the main problem is, with the arduino i am not able to see the sms, but with the terminal i can see the sms so i know theres something wrong with my code. My plan is to read the data into an array and parse the sms message, but i can't read anything into the array if i have no message image. I have uploaded the pic with the terminal showing the sms, any help would be greatly appreciated.


_______________________________________________________________________________________________________________________________

char character=0;

void setup()

{

 

  Serial.begin(9600);

  Serial1.begin(9600);

  delay(60000);

 

 

 

}


void loop()

{

 

 

    int j=0;

  char incoming_let=0;

  char incoming_char[500]=" ";

  String buff1 = String(500);

  Serial1.println("AT+CMGF=1");

  delay(1500);

  Serial1.print("AT+CMGL=");

  Serial1.write((byte)34);

  Serial1.print("ALL");

  Serial1.write((byte)34);

  Serial1.println();

  delay(1000);

 

  while(Serial1.available())

  {

    character = Serial1.read();

   

    Serial.print(character);

  }

 

 

 

}

_____________________________________________________________________________________________________________________________


Output:

+SIND: 11


+SIND: 3


+SIND: 4


OK

+CMGL: 1,0,"REC READ

OK

+CMGL: 1,0,"REC READ","+18687914655","13/03/21,20:39:00+0

OK

+CMGL: 1,0,"REC READ","+18687914655","13/03/21,20:39:00+0

OK

+CMGL: 1,0,"REC READ","+18687914655","13/03/21,20:39:00+0

OK

+CMGL: 1,0,"REC READ","+18687914655","13/03/21,20:39:00+0

OK

+CMGL: 1,0,"REC READ","+18687914655","13/03/21,20:39:00+0

Attachments: