Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino Project: Interactive Shop Window. Help needed.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 420 subscribers
  • Views 984 views
  • Users 0 members are here
  • help
  • led
  • engineering
  • electrical
  • arduino
Related

Arduino Project: Interactive Shop Window. Help needed.

herrlichakafool
herrlichakafool over 13 years ago

Hello element14 community!

 

I want to ask for your opinions about an interactive shop window controlled with an Arduino, but first I try to give you an idea about my technical knowledge.

 

Me and my roommate are studying Games Engineering at the Technical University of Munich, and a friend of ours owns a small clothing shop in Munich.

Since we have sucessfully finished an Arduino project before, he asked us if we can create something special for his shop window.

Our knowledge about circuits and Arduinos is between basic and advanced, so i thought it would be great if some more advanced users can help us out a bit.

 

Here is the idea:

 

The shop window will display 8 to 10 wooden racks, each with 3 slots. In these slots we will put in shoes that we want to promote.

 

                         image

 

Every rack has its own IR sensor, and each slot has 2 LED bars. (bottom row green, middle yellow, top red)

Now when a passenger walks past our window, the IR sensors detect the position of where he stands, and illuminates

the shoe rack in front of him up in all 3 colors, while the once left and right are either yellow and green or just green, which

makes an equalizer effect when you walk past it.

 

Now, what we thought was to control the lighting of each slot with transistors, which are controlled by an Arduino Mega.

 

Now our questions to you guys:

 

1. Is it possible to use IR sensors through a glass window? If the answer is yes, how can we locate a passenger correctly without getting

    signals from more than 1 sensor? If it is "no", what other technology can we use?

 

2. Lets say we use two 12V LED strips, what sort of transistors do we need for that? Or is it dependant on more specifications like resistance?

 

3. What problems can occur during our project? We don't have much experience, but we have all the tools needed.

 

 

I hope that someone can give us a helping hand in this, and that my crappy sketch didn't scare you away image

Also thanks to Ben Heck, otherwise i wouldn't know about element14!

 

Sincerely,

Theo

  • Sign in to reply
  • Cancel

Top Replies

  • kjhart0133
    kjhart0133 over 13 years ago +1
    Just a couple of comments: 1. Infrared radiation generally does not pass through ordinary glass. This is not an absolute and depends chiefly on thickness of the glass and wavelength of the incident IR…
  • mcb1
    mcb1 over 13 years ago in reply to herrlichakafool +1
    Theo If you mounted your IR sensors inside a metal tube that ran along the top (or the bottom) of the window (outside) you could angle them to reduce the range. You could also try mounting a TX that flooded…
  • billabott
    billabott over 13 years ago +1
    Okay, here's an outside the box idea for your project. Put a puppy in the window! It tracks the people and the sensors track the dog. No drilling needed.
Parents
  • billabott
    billabott over 13 years ago

    Okay, here's an outside the box idea for your project.  Put a puppy in the window!  It tracks the people and the sensors track the dog.  No drilling needed.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • billabott
    billabott over 13 years ago

    Okay, here's an outside the box idea for your project.  Put a puppy in the window!  It tracks the people and the sensors track the dog.  No drilling needed.