Arduino Forum RF transmitter
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
  • Replies 11 replies
  • Subscribers 393 subscribers
  • Views 800 views
  • Users 0 members are here
Related

RF transmitter

Former Member
Former Member over 9 years ago

Hi all,can anybody help me about code for send image via RF transmitter using arduino uno or mega

and the image store in SD card  shield or memory interne in arduino

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 9 years ago +2
    Let me google that for you
Parents
  • Former Member
    Former Member over 9 years ago

    It would have been useful to know what the overall project/application is.  Also, where is the transmission occurring and for what distance?  As several folks have pointed out, RF transmission has its downside for various reasons.

     

    If your receiver is always close to the Arduino transmitter (E.g. you could wait until this was true), then one reliable and relatively cheap way to proceed is to create a point-to-point connection using a cross RS-232C cable, either real or (more fun----->) simulated through a breadboard as in https://www.arduino.cc/en/Tutorial/ArduinoSoftwareRS232.  At that URL, you can read the 1970s technology that still works brilliantly.  I won't steal your fun.  In a nutshell, one end is the "data terminal" (E.g. Arduino) and the other end is the "host" (E.g. a PC).

     

    For extra credit and fun, make a permanent cross RS-232C cable with DB-9 connectors at each end.

     

    What do you think about that?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 9 years ago

    It would have been useful to know what the overall project/application is.  Also, where is the transmission occurring and for what distance?  As several folks have pointed out, RF transmission has its downside for various reasons.

     

    If your receiver is always close to the Arduino transmitter (E.g. you could wait until this was true), then one reliable and relatively cheap way to proceed is to create a point-to-point connection using a cross RS-232C cable, either real or (more fun----->) simulated through a breadboard as in https://www.arduino.cc/en/Tutorial/ArduinoSoftwareRS232.  At that URL, you can read the 1970s technology that still works brilliantly.  I won't steal your fun.  In a nutshell, one end is the "data terminal" (E.g. Arduino) and the other end is the "host" (E.g. a PC).

     

    For extra credit and fun, make a permanent cross RS-232C cable with DB-9 connectors at each end.

     

    What do you think about that?