Arduino
  • Products
  • More
Arduino
Arduino Forum W5200 Ethernet Shield for Arduino, bring your smart appliance to the internet
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 415 subscribers
  • Views 290 views
  • Users 0 members are here
  • ethernet
  • shield
Related

W5200 Ethernet Shield for Arduino, bring your smart appliance to the internet

e14 Contributor
e14 Contributor over 13 years ago

I have found this message on eevblog,  I bring it here, hope you find this useful.

 

Hi all,

W5200 Ethernet Shield in Elecrow is available now!


image

 

image



The controller of this Ethernet Shield is W5200. it is twice the buffer size of W5100 and support for up to eight simultaneous TCP/UDP connections. There is an onboard micro-SD card slot, which can be used to store files for serving over the network. Thanks to a lowered RJ45 pot, you can flexibly add most shields on top of this Ethernet Shield.


Features:

  • Standard Shield that Arduino, Mega, Crowduino Compatible
  • High speed Ethernet controller W5200 with internal 32K buffer
  • With Micro SD card for storing large amounts of data
  • Connection with Arduino on SPI port
  • Support up to eight simultaneous TCP/UDP connections
  • Lowered RJ45 Ethernet jack
  • Long wire-wrap headers extend through the shield

For more details please vistit Elecrow W5200 Ethernet Shield.