Arduino
  • Products
  • More
Arduino
Arduino Forum Problems with Sparkfun micro SD card + Arduino 2560( gps data logging)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 415 subscribers
  • Views 313 views
  • Users 0 members are here
Related

Problems with Sparkfun micro SD card + Arduino 2560( gps data logging)

e14 Contributor
e14 Contributor over 13 years ago

Hello all,


I am very far in my current project. Now, I am at a crossroads. I am using a micro sd card shield from Sparkfun with a Ardunio Mega 2560. I am making a data logger for my GPS module. I used the code from Jeremy Blum's tutorial for GPS Receiver(data logging portion).

 

//Jeremy Blum's Arduino Tutorial Series - Episode 15 - GPS Tracking

//Sample Code 2 - Logging GPS Data to an SD Card

//http://www.jeremyblum.com

//TinyGPS Library and Helper Functions by Mikal Hart http://arduiniana.org/libraries/tinygps/

 

 

 

 

#include <TinyGPS.h>

#include <SD.h>

#include <stdlib.h>

 

 

/* This sample code demonstrates the normal use of a TinyGPS object.

   It uses an Arduino Mega with a GPS attached to Serial3 at 57600 buad.

*/

 

 

TinyGPS gps;

static char dtostrfbuffer[20];

int CS = 53;

int LED = 13;

 

 

//Define String

String SD_date_time = "invalid";

String SD_lat = "invalid";

String SD_lon = "invalid";

String dataString ="";

 

 

static void gpsdump(TinyGPS &gps);

static bool feedgps();

static void print_float(float val, float invalid, int len, int prec, int SD_val);

static void print_int(unsigned long val, unsigned long invalid, int len);

static void print_date(TinyGPS &gps);

static void print_str(const char *str, int len);

 

 

void setup()

{

  pinMode(CS, OUTPUT);  //Chip Select Pin for the SD Card

  pinMode(LED, OUTPUT);  //LED Indicator

 

  //Serial interfaces

  Serial.begin(115200);

  Serial3.begin(57600);

 

  //Connect to the SD Card

  if(!SD.begin(CS))

  {

    Serial.println("Card Failure");

    return;

  }

 

 

  Serial.print("Testing TinyGPS library v. "); Serial.println(TinyGPS::library_version());

  Serial.println("by Mikal Hart");

  Serial.println();

  Serial.print("Sizeof(gpsobject) = "); Serial.println(sizeof(TinyGPS));

  Serial.println();

  Serial.println("Sats HDOP Latitude Longitude Fix  Date       Time       Date Alt     Course Speed Card  Distance Course Card  Chars Sentences Checksum");

  Serial.println("          (deg)    (deg)     Age                        Age  (m)     --- from GPS ----  ---- to London  ----  RX    RX        Fail");

  Serial.println("--------------------------------------------------------------------------------------------------------------------------------------");

}

 

 

void loop()

{

  bool newdata = false;

  unsigned long start = millis();

 

  // Every second we print an update

  while (millis() - start < 1000)

  {

    if (feedgps())

      newdata = true;

  }

 

  gpsdump(gps);

 

  //Write the newest information to the SD Card

  dataString = SD_date_time + "," + SD_lat + "," + SD_lon;

  if(SD_date_time != "invalid")

    digitalWrite(LED, HIGH);

  else

    digitalWrite(LED, LOW);

 

  //Open the Data CSV File

  File dataFile = SD.open("LOG.csv", FILE_WRITE);

  if (dataFile)

  {

    dataFile.println(dataString);

    Serial.println(dataString);

    dataFile.close();

  }

  else

  {

    Serial.println("\nCouldn't open the log file!");

  }

}

 

 

static void gpsdump(TinyGPS &gps)

{

  float flat, flon;

  unsigned long age, date, time, chars = 0;

  unsigned short sentences = 0, failed = 0;

  static const float LONDON_LAT = 51.508131, LONDON_LON = -0.128002;

 

  print_int(gps.satellites(), TinyGPS::GPS_INVALID_SATELLITES, 5);

  print_int(gps.hdop(), TinyGPS::GPS_INVALID_HDOP, 5);

  gps.f_get_position(&flat, &flon, &age);

  print_float(flat, TinyGPS::GPS_INVALID_F_ANGLE, 9, 5, 1); //LATITUDE

  print_float(flon, TinyGPS::GPS_INVALID_F_ANGLE, 10, 5, 2); //LONGITUDE

  print_int(age, TinyGPS::GPS_INVALID_AGE, 5);

 

 

  print_date(gps); //DATE AND TIME

 

 

  print_float(gps.f_altitude(), TinyGPS::GPS_INVALID_F_ALTITUDE, 8, 2, 0);

  print_float(gps.f_course(), TinyGPS::GPS_INVALID_F_ANGLE, 7, 2, 0);

  print_float(gps.f_speed_kmph(), TinyGPS::GPS_INVALID_F_SPEED, 6, 2, 0);

  print_str(gps.f_course() == TinyGPS::GPS_INVALID_F_ANGLE ? "*** " : TinyGPS::cardinal(gps.f_course()), 6);

  print_int(flat == TinyGPS::GPS_INVALID_F_ANGLE ? 0UL : (unsigned long)TinyGPS::distance_between(flat, flon, LONDON_LAT, LONDON_LON) / 1000, 0xFFFFFFFF, 9);

  print_float(flat == TinyGPS::GPS_INVALID_F_ANGLE ? 0.0 : TinyGPS::course_to(flat, flon, 51.508131, -0.128002), TinyGPS::GPS_INVALID_F_ANGLE, 7, 2, 0);

  print_str(flat == TinyGPS::GPS_INVALID_F_ANGLE ? "*** " : TinyGPS::cardinal(TinyGPS::course_to(flat, flon, LONDON_LAT, LONDON_LON)), 6);

 

 

  gps.stats(&chars, &sentences, &failed);

  print_int(chars, 0xFFFFFFFF, 6);

  print_int(sentences, 0xFFFFFFFF, 10);

  print_int(failed, 0xFFFFFFFF, 9);

  Serial.println();

}

 

 

static void print_int(unsigned long val, unsigned long invalid, int len)

{

  char sz[32];

  if (val == invalid)

    strcpy(sz, "*******");

  else

    sprintf(sz, "%ld", val);

  sz[len] = 0;

  for (int i=strlen(sz); i<len; ++i)

    sz[i] = ' ';

  if (len > 0)

    sz[len-1] = ' ';

  Serial.print(sz);

  feedgps();

}

 

 

static void print_float(float val, float invalid, int len, int prec, int SD_val)

{

  char sz[32];

  if (val == invalid)

  {

    strcpy(sz, "*******");

    sz[len] = 0;

        if (len > 0)

          sz[len-1] = ' ';

    for (int i=7; i<len; ++i)

        sz[i] = ' ';

    Serial.print(sz);

    if(SD_val == 1) SD_lat = sz;

    else if(SD_val == 2) SD_lon = sz;

  }

  else

  {

    Serial.print(val, prec);

    if (SD_val == 1) SD_lat = dtostrf(val,10,5,dtostrfbuffer);

    else if (SD_val == 2) SD_lon = dtostrf(val,10,5,dtostrfbuffer);

    int vi = abs((int)val);

    int flen = prec + (val < 0.0 ? 2 : 1);

    flen += vi >= 1000 ? 4 : vi >= 100 ? 3 : vi >= 10 ? 2 : 1;

    for (int i=flen; i<len; ++i)

      Serial.print(" ");

  }

  feedgps();

}

 

 

static void print_date(TinyGPS &gps)

{

  int year;

  byte month, day, hour, minute, second, hundredths;

  unsigned long age;

  gps.crack_datetime(&year, &month, &day, &hour, &minute, &second, &hundredths, &age);

  if (age == TinyGPS::GPS_INVALID_AGE)

  {

    Serial.print("*******    *******    ");

    SD_date_time = "invalid";

  }

  else

  {

    char sz[32];

    sprintf(sz, "%02d/%02d/%02d %02d:%02d:%02d   ",

        month, day, year, hour, minute, second);

    Serial.print(sz);

    SD_date_time = sz;

  }

  print_int(age, TinyGPS::GPS_INVALID_AGE, 5);

  feedgps();

}

 

 

static void print_str(const char *str, int len)

{

  int slen = strlen(str);

  for (int i=0; i<len; ++i)

    Serial.print(i<slen ? str[i] : ' ');

  feedgps();

}

 

 

static bool feedgps()

{

  while (Serial3.available())

  {

    if (gps.encode(Serial3.read()))

      return true;

  }

  return false;

}

 

 

When I connect the shield to a separate breadboard and jumper it to the Arduino it works fine. But when I mount the shield to the Arduino(pins are lined up), I get this error in the serial monitor, "Couldn't open the log file!". There is nothing wrong with the sd card and I wired everything correctly. What am I doing wrong? Should I insert the shield to a Uno instead?

 

Also, the pin outputs are below

 

2560   sd shield

D50 -->  MISO (12)

D51 -->  MOSI (11)

D52 -->  SCK (13)

D53 -->  CS (eight)

3.3V --> 3.3V

GND --> GND