Arduino
  • Products
  • More
Arduino
Arduino Forum I2C does not send all data
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 416 subscribers
  • Views 449 views
  • Users 0 members are here
  • i2c
Related

I2C does not send all data

e14 Contributor
e14 Contributor over 13 years ago

I am using a Arduino Nano Rev 3.1 with Arduino.exe 1.0.4 with a I2C LED control chip

I need to send the chip address, a LED address and 2 bytes of data.  I found the Wire.h library and a bunch of web pages and tutorials but I can’t make it work. I am beginning to wonder if the Nano I am using is damaged.

The reference  for Wire.h indicate there will be pull ups on the clock and data, but I did not have them and added resistors.

The reference for Wire.h indicates it will append a 1 as the most significant address bit on the address, my first address bit is always a zero even if I set the address to 0x80.

My sketch sends the address and 3 data bytes.  All I see on the scope is an address byte without the MSB set, my control byte, the first byte of data, then end of message.

I am looking for any advice, is it software, is it a damaged Nano.

 

/******************************************************

Arduino Nano I2C test

5/4/2013

*******************************************************/

// Arduino Nano A4 is I2C SDA

// Arduino Nano A5 is I2C SCL

//Nano is a rev 3.1 Arduino.exe is 1.0.4

#include "Wire.h"

 

void setup()             // run once, when the sketch starts

{

  Wire.begin();          //start wire library for I2C

  delay(20);

}

 

void loop(void)

{

int i=0, j=0, k=0;

digitalWrite(2, LOW);   // chip enable

 

while(1)

    {

    SendLED();

    delay(5);

   }

}

 

void SendLED(void)

{

  1. Wire.beginTransmission(0);    //chip address
  2. Wire.write(3);                //send LED address
  3. Wire.write(15);               //send low data byte
  4. Wire.write(63);               //send hi data byte
  5. Wire.endTransmission();       //end command

}

  • Sign in to reply
  • Cancel
  • shabaz
    shabaz over 13 years ago

    Hi David,

     

    I didn't read the entire code, but the first key thing is that the address is not correct. As I understand, the documentation says that it expects a 7-bit address (which it will left-shift by one bit position, and then the LSB controls the read/write operation).

    Setting it to 0x80 is not good, because the left-shift operation will make it become zero.

    If your LED driver is expecting address 0x80, then the value to use is 0x40; it will get left-shifted to become 0x80.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz

    Thank you shabaz for the tip about the address getting shifted.

    I entered 0x40  for the address and the address showed up on the data but I was still not getting all 4 bytes showing up on the data lines.  I reviewed the instructions for the salve device and found that address 0x40 was a reset command.  I changed the address to 0x41 and moved A1 on the chip to be a high and I got 4 bytes of I2C data and the chip worked as expected.

    Thanks David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to e14 Contributor

    Excellent, glad it works!