Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino drop-in IEEE 802.15.4 radio module
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 4 replies
  • Subscribers 417 subscribers
  • Views 1294 views
  • Users 0 members are here
  • sensors_expo
  • colorado
  • arm_cortex_m0
  • chicago
  • wireless
  • nxp
  • arduino
  • 802.15.4
  • atmel
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

Arduino drop-in IEEE 802.15.4 radio module

fustini
fustini over 13 years ago

I attended the Sensors Expo in Chicago this afternoon.  One of the interesting devices I came across was RadioBlocks from Colorado Microdevices:

The Colorado Micro Devices RadioBlock is an IEEE 802.15.4 FCC and CE certified wireless modem. It has a simple UART interface to make it easy to drop into your end product or to experiment with. A standard 100 mil pin spaced header means you can plug it right into many common boards: Arduino, Raspberry Pi, BeagleBone, it’s easy – No special pin configuration or adapter board needed!

I blogged about how it can be used directly with the Raspberry Pi (RadioBlocks: drop-in IEEE 802.15.4 wireless module for Raspberry Pi) but it also fits the Arduino quite nicely:

 

image

I'm not very familiar with the inner workings of IEEE 802.15.4 but RadioBlocks claims to make it simple to configure and use. 

 

Has anyone used similar devices?

Do you think this is a useful board?

 

Cheers,

Drew

http://twitter.com/pdp7

  • Cancel

Top Replies

  • mcb1
    mcb1 over 13 years ago +1
    The boys/girls have also gotten them to work on Digisparks as well. http://digistump.com/board/index.php/topic,64.msg3587.html#msg3587 They do look very interesting, and an alternative to the Nordic offerings…
  • fustini
    fustini over 12 years ago +1
    Who wants RadioBlocks (Simple Radio for Arduino)? I'm giving them away!
Parents
  • fustini
    fustini over 12 years ago

    Who wants RadioBlocks (Simple Radio for Arduino)?  I'm giving them away!

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
Reply
  • fustini
    fustini over 12 years ago

    Who wants RadioBlocks (Simple Radio for Arduino)?  I'm giving them away!