Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino for my Father's Model Railroad Layout
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 420 subscribers
  • Views 1412 views
  • Users 0 members are here
Related

Arduino for my Father's Model Railroad Layout

e14 Contributor
e14 Contributor over 13 years ago

Hi there, I'm looking to do a little brainstorming for an idea I had involving the Model Railroad my Dad built in his basement.

 

There's 2 things I want to do.

 

1. add sound to the scenery - He has a DCC layout which gives sound to the trains themselves... but I want to add sound to the scenery.

i.e the waterfall in the corner... or the some birds in the forest... even the sound of mechanics hammering away in the maintanence yard/engine house.

 

2. Arduino controlled signal lights for sections of track based on trains in the area...

i.e Say there are 4 blocks of consecutive track - A B C D. if a train enters track block D the signal for following trains into block D should be red. the signal for block C should be amber and the signals for B should be green. It also get a little more complicated when adding track switch positions into the mix...

 

For Goal number 1 the idea would be that sounds don't play until you're standing infront of the scene. I'm not sure whether to use IR Sharp Distance sensor or a cheap Ultrasonic sensor as the triggering device. And then I don't know what to use to play the sounds.. It would need to be small speakers that can be hidden in the scenery.. I'm thinking no bigger than the size of a quarter. And then what stores and plays the sounds?

 

Goal number 2 has LED's embedded throughout the layout... some signals would be flag type signals requiring servos to move the position of the flag... My biggest problem is how do you detect the train's position on the track?

 

I want to figure out the hardware situation first, then I can start worrying about writting the programs...

I'm thinking the 2 operatons would require their own processors (2 arduino control boards) Unless it is possible to have one board control everything. But I don't know.

 

Any ideas would be great.

 

Thanks,

Guido

  • Sign in to reply
  • Cancel

Top Replies

  • billabott
    billabott over 13 years ago +1
    Okay. Great. Borrow some ideas from this guy: http://70.66.73.1/arduino.html
Parents
  • mcb1
    mcb1 over 13 years ago

    Guy

    You have presented a well thoughtout project with good information to assist.

     

    In reverse

    2. Detection

    There are 'Hall effect' switches that detect a magnet pasing them.

    You could fit these under the train.

     

    There are also optical sensors that will see the Infra Red beam refected off a surface of the train, that can be fitted underneath.

    You could also detect the ambient light, and when the train passes over it is detected.

     

    Both are a dollar or two.

     

    1. Sounds

    The Arduino can play sounds, but a simple sound bite device (similar to the internals in childrens toys or greeting cards) is probably the easiest.

    I'm sure there are some MP3 style shields avavilable to play sounds from an SD card, which may suit your budget as well.

    Depending on which method you choose, it is relatively easy to do.

     

    The ultrasonics work well, and you can set the maximum distance, to avoid false triggering.

     

     

    I suggest you can start working on your code/sketch with a some simple switches and leds.

    There are examples within the IDE, and plenty of books and tutorials that have been suggested here before.  (search works)

     

    I suggest trying to avoid using delay() and master the "BlinkWithoutDelay" example that uses the millis() timer instead of delay.

     

    mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mcb1
    mcb1 over 13 years ago

    Guy

    You have presented a well thoughtout project with good information to assist.

     

    In reverse

    2. Detection

    There are 'Hall effect' switches that detect a magnet pasing them.

    You could fit these under the train.

     

    There are also optical sensors that will see the Infra Red beam refected off a surface of the train, that can be fitted underneath.

    You could also detect the ambient light, and when the train passes over it is detected.

     

    Both are a dollar or two.

     

    1. Sounds

    The Arduino can play sounds, but a simple sound bite device (similar to the internals in childrens toys or greeting cards) is probably the easiest.

    I'm sure there are some MP3 style shields avavilable to play sounds from an SD card, which may suit your budget as well.

    Depending on which method you choose, it is relatively easy to do.

     

    The ultrasonics work well, and you can set the maximum distance, to avoid false triggering.

     

     

    I suggest you can start working on your code/sketch with a some simple switches and leds.

    There are examples within the IDE, and plenty of books and tutorials that have been suggested here before.  (search works)

     

    I suggest trying to avoid using delay() and master the "BlinkWithoutDelay" example that uses the millis() timer instead of delay.

     

    mark