Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino for my Father's Model Railroad Layout
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 420 subscribers
  • Views 1408 views
  • Users 0 members are here
Related

Arduino for my Father's Model Railroad Layout

e14 Contributor
e14 Contributor over 13 years ago

Hi there, I'm looking to do a little brainstorming for an idea I had involving the Model Railroad my Dad built in his basement.

 

There's 2 things I want to do.

 

1. add sound to the scenery - He has a DCC layout which gives sound to the trains themselves... but I want to add sound to the scenery.

i.e the waterfall in the corner... or the some birds in the forest... even the sound of mechanics hammering away in the maintanence yard/engine house.

 

2. Arduino controlled signal lights for sections of track based on trains in the area...

i.e Say there are 4 blocks of consecutive track - A B C D. if a train enters track block D the signal for following trains into block D should be red. the signal for block C should be amber and the signals for B should be green. It also get a little more complicated when adding track switch positions into the mix...

 

For Goal number 1 the idea would be that sounds don't play until you're standing infront of the scene. I'm not sure whether to use IR Sharp Distance sensor or a cheap Ultrasonic sensor as the triggering device. And then I don't know what to use to play the sounds.. It would need to be small speakers that can be hidden in the scenery.. I'm thinking no bigger than the size of a quarter. And then what stores and plays the sounds?

 

Goal number 2 has LED's embedded throughout the layout... some signals would be flag type signals requiring servos to move the position of the flag... My biggest problem is how do you detect the train's position on the track?

 

I want to figure out the hardware situation first, then I can start worrying about writting the programs...

I'm thinking the 2 operatons would require their own processors (2 arduino control boards) Unless it is possible to have one board control everything. But I don't know.

 

Any ideas would be great.

 

Thanks,

Guido

  • Sign in to reply
  • Cancel

Top Replies

  • billabott
    billabott over 13 years ago +1
    Okay. Great. Borrow some ideas from this guy: http://70.66.73.1/arduino.html
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    A bit late but better late than never. 

     

    There are 3 ways to detect the trains - current detection, infrared, optical. 

     

    For trains on a section of track (eg to trigger trackside signals, level crossing signals), current detection works best.  Current detection requires an insulated section of track that can detect current flow when the train moves into the insulated section.  There are several off-the-shelf products that can do this, the best one being the NCE BD20 block detector.  (NCE - North Coast Engineering).  These units present a logic 1 when current flows. 

     

    Similar results can be produced with infrared detectors and optical detectors, although both are sensitive to ambient light (room lighting) and can be a real pain in the posterior.  However, the Arduino can be a good controller as you can program it with debounce functions.  For IR, there are two types of detection - cutting the IR beam, and bouncing the IR beam back to the IR detector.  Cutting the IR beam units are placed on each side of the track.  Bouncing IR beams are placed in the middle of the track so that the beam bounces off the underside of the cars going over the unit.  Optical detectors simply cut the beam. 

     

    For both IR and optical detectors, units are placed at the limits of the stretch of track where detection is required (eg on both sides of a level crossing) with the units connected to the Arduino.  As long as both or either one are detecting, the signals are operating.  Again, you will have to incorporate debounce functions in your programming. 

     

    For trackside signals, you are starting to get into some fairly complex arrangements.  A straight piece of track is relatively easy to program.  However, when you get into turnouts (aka switches) where the track goes off in two (or more) directions), things get a bit complicated.  For a turnout, this requires a mechanical switch at the turnout which can indicate which way the track is aligned. 

     

    Don't know if this helps but it's a start.  My suggestion would be to begin with a simple level crossing with some flashing lights.  Then add a bell, followed by some crossing gates connected to a servo. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 11 years ago

    A bit late but better late than never. 

     

    There are 3 ways to detect the trains - current detection, infrared, optical. 

     

    For trains on a section of track (eg to trigger trackside signals, level crossing signals), current detection works best.  Current detection requires an insulated section of track that can detect current flow when the train moves into the insulated section.  There are several off-the-shelf products that can do this, the best one being the NCE BD20 block detector.  (NCE - North Coast Engineering).  These units present a logic 1 when current flows. 

     

    Similar results can be produced with infrared detectors and optical detectors, although both are sensitive to ambient light (room lighting) and can be a real pain in the posterior.  However, the Arduino can be a good controller as you can program it with debounce functions.  For IR, there are two types of detection - cutting the IR beam, and bouncing the IR beam back to the IR detector.  Cutting the IR beam units are placed on each side of the track.  Bouncing IR beams are placed in the middle of the track so that the beam bounces off the underside of the cars going over the unit.  Optical detectors simply cut the beam. 

     

    For both IR and optical detectors, units are placed at the limits of the stretch of track where detection is required (eg on both sides of a level crossing) with the units connected to the Arduino.  As long as both or either one are detecting, the signals are operating.  Again, you will have to incorporate debounce functions in your programming. 

     

    For trackside signals, you are starting to get into some fairly complex arrangements.  A straight piece of track is relatively easy to program.  However, when you get into turnouts (aka switches) where the track goes off in two (or more) directions), things get a bit complicated.  For a turnout, this requires a mechanical switch at the turnout which can indicate which way the track is aligned. 

     

    Don't know if this helps but it's a start.  My suggestion would be to begin with a simple level crossing with some flashing lights.  Then add a bell, followed by some crossing gates connected to a servo.