Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino for my Father's Model Railroad Layout
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 420 subscribers
  • Views 1414 views
  • Users 0 members are here
Related

Arduino for my Father's Model Railroad Layout

e14 Contributor
e14 Contributor over 13 years ago

Hi there, I'm looking to do a little brainstorming for an idea I had involving the Model Railroad my Dad built in his basement.

 

There's 2 things I want to do.

 

1. add sound to the scenery - He has a DCC layout which gives sound to the trains themselves... but I want to add sound to the scenery.

i.e the waterfall in the corner... or the some birds in the forest... even the sound of mechanics hammering away in the maintanence yard/engine house.

 

2. Arduino controlled signal lights for sections of track based on trains in the area...

i.e Say there are 4 blocks of consecutive track - A B C D. if a train enters track block D the signal for following trains into block D should be red. the signal for block C should be amber and the signals for B should be green. It also get a little more complicated when adding track switch positions into the mix...

 

For Goal number 1 the idea would be that sounds don't play until you're standing infront of the scene. I'm not sure whether to use IR Sharp Distance sensor or a cheap Ultrasonic sensor as the triggering device. And then I don't know what to use to play the sounds.. It would need to be small speakers that can be hidden in the scenery.. I'm thinking no bigger than the size of a quarter. And then what stores and plays the sounds?

 

Goal number 2 has LED's embedded throughout the layout... some signals would be flag type signals requiring servos to move the position of the flag... My biggest problem is how do you detect the train's position on the track?

 

I want to figure out the hardware situation first, then I can start worrying about writting the programs...

I'm thinking the 2 operatons would require their own processors (2 arduino control boards) Unless it is possible to have one board control everything. But I don't know.

 

Any ideas would be great.

 

Thanks,

Guido

  • Sign in to reply
  • Cancel

Top Replies

  • billabott
    billabott over 13 years ago +1
    Okay. Great. Borrow some ideas from this guy: http://70.66.73.1/arduino.html
Parents
  • dtozer
    dtozer over 11 years ago

    Take a look at ESU dcc sound decoders, the the Select, USA version.

    This system the decoders you program the sound files.

    I am sure they will assist you and make recommendations.

    Use speakers of no less than 1 inch and in an enclosure to enhance the sound.

    You loose a lot of quality and db's when you do not use the correct enclosure for the speaker and the correct type for the frequency range you are trying to recreate.

    Hope this helps!

    Regards

    David Tozer

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dtozer
    dtozer over 11 years ago

    Take a look at ESU dcc sound decoders, the the Select, USA version.

    This system the decoders you program the sound files.

    I am sure they will assist you and make recommendations.

    Use speakers of no less than 1 inch and in an enclosure to enhance the sound.

    You loose a lot of quality and db's when you do not use the correct enclosure for the speaker and the correct type for the frequency range you are trying to recreate.

    Hope this helps!

    Regards

    David Tozer