Arduino
  • Products
  • More
Arduino
Arduino Forum I need help with arduino lcd shield with Ethenet/SD shield conflict.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 417 subscribers
  • Views 447 views
  • Users 0 members are here
  • lcd
  • conflict.
  • ethenet/sd
  • shield
  • arduino
Related

I need help with arduino lcd shield with Ethenet/SD shield conflict.

e14 Contributor
e14 Contributor over 13 years ago

Dear Gurus,

 

I am using an arduino mega2560 with an ethernet/SD card shield. I need to include a display shield but most of the ones I've seen have conflicts with pin 10 (ethernet) or pin 4(SD card). Also, they dont sit well on the ethernet shield because the ehternet port is too big on the board. Do you know of any LCD shield that won't give me any of these troubles?

Thanks

  • Sign in to reply
  • Cancel
Parents
  • mcb1
    mcb1 over 13 years ago

    Oludamilare

    You've asked the same question multiple times.

    This is not good forum manners.

     

    You could go back and delete the extra versions, and keep the one that has been posed here.

     

    You might then have a better chance of an answer, and make it easier for someone with a similar query to find a solution.

     

    I have seen the use of double header plugs to raise the shield.

    You could always use an I2C LCD which is probably cheaper and allows the display to be rotated or fitted an any angle.

    It also saves on pins, which may allow the use of a standard Arduino.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to mcb1

    Thanks a lot. I have deleted the duplicate questions. Thanks for the response.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to mcb1

    Thanks a lot. I have deleted the duplicate questions. Thanks for the response.