Arduino
  • Products
  • More
Arduino
Arduino Forum PWM in arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 418 subscribers
  • Views 567 views
  • Users 0 members are here
  • arduino
Related

PWM in arduino

tejaswivarma
tejaswivarma over 13 years ago

Hi,

      I am Varma from India. I am working on arduino. i want to generate a PWM signal with time of 40 mSec. how should I change the time ????

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago +1
    http://arduino.cc/en/Tutorial/SecretsOfArduinoPWM It seems you might have to do some calculations to see if you can get that value out of an arduino. Good luck.
  • e14 Contributor
    e14 Contributor over 13 years ago

    http://arduino.cc/en/Tutorial/SecretsOfArduinoPWM

     

    It seems you might have to do some calculations to see if you can get that value out of an arduino.  Good luck.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • deeps
    deeps over 11 years ago

    Hi

    u want 40ms time period in your pwm

    But what duty cycle do u want?

    see time period is on time + off time

    I think u want 50% duty cycle

    so 20ms on time

    and 20ms off time

    you can simply use digital write and delay

    similar to blink program but your delay will be according to on time and off time

    the delay after writing high in the pin is your on time

    and that after writing low is your off time

    Hope it helped

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to deeps

    I would suggest you use the pwm library for this purpose as using delay() will cause all processing to suspend while the delay is going on, this is ok if the only think you want the Arduino to do is output the PWM signal but is now good once you want to do other things

     

     

     

    The PWM library allows you do do other things and makes setting the parameters much simpler

     

     

     

     

     

    See http://arduino.cc/en/Tutorial/SecretsOfArduinoPWM

     

    And

     

    https://code.google.com/p/arduino-pwm-frequency-library/

     

     

     

    Hope this helps

     

     

     

    Peter

    Attachments:
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • deeps
    deeps over 11 years ago in reply to Robert Peter Oakes

    Well a solution to the problem with delay

    is with using milllis()

     

    https://learn.adafruit.com/multi-tasking-the-arduino-part-1/now-for-two-at-once

    With this we can multi thread arduino (kindof)

    and prevent arduino from suspending when delay is required

    and with all due respect sir

    I dont like using libraries too much

    1 they consume lots of space the functions that you may not require too come into rom

    2 It makes it hard to optimize your system which is first priority of modern embedded system design

    3 you are unable to understand the details of what is happening for example lcd seems easy but study how its to be done in ALP and than see the library of lcd and you will start to understand the details which the library was hiding from you