Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino + Driver Board & Stepper motor
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 418 subscribers
  • Views 1477 views
  • Users 0 members are here
Related

Arduino + Driver Board & Stepper motor

e14 Contributor
e14 Contributor over 12 years ago

Hi everyone,

 

I wonder if anyone can help me, I'm trying to build a 'Barn Door tracker mount' (see - http://500px.com/eliperelman/stories/60797 )

 

I'm totally confussed, as I was told that you need a Driver Board to be wired into the Arduino... but the guy in that link above seems to have wired the motor directly into the Arduino, also, Im not sure how he's powering it? (Would it be a 9v battery?)

 

I have an Arduino and a driver board + stepper motor... all the gear and no idea! lol

 

Any help would really be appreciated.

 

Thank you.

  • Sign in to reply
  • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to e14 Contributor

    Stuart

    this line here gives you the answer I think you're looking for

     

    myStepper.setSpeed(60);

     

    it even says so above it.

      // set the speed at 60 rpm:

     

    Have you tried it?

     

    Does this motor take 200 pulses to do a full revolution.?

    From the limited information this supplier gave (despite suggesting they had a forum)

    Step angle: 5.625 x 1/64
        Reduction ratio: 1/64

     

    Comparing it with the others from the same factory that are a little clearer, the stepper motor is 5.625 deg and a 64:1 reduction.

     

    360 deg divided by 5.625 deg = 64.

    It also has a 64:1 ratio reduction, so therefore 64 x 64 = 4096 steps for a full revolution.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to mcb1

    Hi Mark, yeah it was set to 60.

     

    To be honest, I think I've got in a complete muddle lol

     

    I was hoping to pinch the example sketch and just tweak it, but I can't seem to get it to work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to e14 Contributor

    Stuart.

     

    You need to check to see what is happening, before you can rectify the problem.

     

    As you know delay(1000) adds a one second delay before moving to the next instruction.

     

    I would change this

    const int stepsPerRevolution = 200

    to

    const int stepsPerRevolution = 4096

     

    and this

    myStepper.setSpeed(60);

    to

    myStepper.setSpeed(1);

     

    Uload it and try again.

    It should do one whole revolution, wait 0.5 secs, then reverse (using the code ** with edits** in your post).

     

    The 9 volts is because some motor drivers won't work below 7v, its just the way they are.

    I'm keen to see the end result because I've been asked to do a similar thing ... (except I don't have the scope).

    I was thinking of using the same motor.

     

    mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<