Arduino
  • Products
  • More
Arduino
Arduino Forum LED Night project
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 416 subscribers
  • Views 981 views
  • Users 0 members are here
  • help
  • light
  • needed
  • tm1803
  • led
  • night
  • tri-color
  • arduino
Related

LED Night project

josh_j
josh_j over 12 years ago

Ok so a few months back I posted about this LED night light I'm making for my girlfriend. I decide that instead of getting a bunch of RGB LEDs, I went and bought the Tri-color LED strip instead because it seemed like a idiot proof thing to do. I downloaded the example code for it and it looks great! But here is my trouble, how do I add a dimmer dial to the code?

 

Here is a link to the code.https://github.com/Grid21/_2760339_Program

 

The strip is analog and uses three pins. It plugs into pins GND, VIN and A0 (analog 0) The chip on the strip is a TM1803 chip.

 

I did read over all the .PDF documentation but I still don't understand what I read. If someone here could look at the code, explain to me and then explain how to add a line of code that would use a variable resistor dial to adjust the brightness that would be fantastic! If need be I can also give links to the .PDFs I have on the tri-color LED Strip.

 

Thanks so much for the coming help!
Josh

 

Also could sciguy14 Help me?

Attachments:
image2760339_PM_EN.pdf
imageTM1803.pdf
  • Sign in to reply
  • Cancel
Parents
  • gadget.iom
    gadget.iom over 12 years ago

    OK....

     

    Have had a look into the code, and without any hardware this is difficult to test. But here goes...

     

    add the following code into the 'send_1M_pattern' function just ABOVE the 'send_strip(temp_data)' line.

     

    // Convert Hex to seperate RGB Values

    long r=(long)(temp_data>>16);

    long g=(long)(r>>8);

    long b=(long)temp_data;

     

    // Apply multiplication factor for brightness

    r = (float)r * (a_val/1024.0);

    g = (float)g * (a_val/1024.0);

    b = (float)b * (a_val/1024.0);

     

    // Convert RGB values back to Hex

    long temp_data = ((long)r << 16) | ((long)g << 8 ) | (long)b;

     

     

     

     

     

     

    This code will apply a scaling factor to the output dependent on the value of variable 'a_val' this value should be set through an AnalogueRead on the pin connected to your variable resistor. This AnaglogRead instruction can be added just ABOVE the 'for (i=0;i<pattern_no;i++)' line so that the analogue value is not being polled continuously during the loop.

     

     

    Let me know how you get on.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • josh_j
    josh_j over 12 years ago in reply to gadget.iom

      {
        send_1M_pattern(pattern_test_rainbow, 10, 70);
      }
    
    
    
    
      /*
      frame++;
        if(frame<=10) LEDSTRIP_PATTERN_0();
        if(10<frame<=20) LEDSTRIP_PATTERN_0();
        if(20<frame<=30) LEDSTRIP_PATTERN_0();
        if(frame>30) frame=1;
       */
      //delay(1);
    }
    
    
    
    
    /*******************************************************************************
     * Function Name  : send_1M_pattern
     * Description    : Transmit pattern to whole 1 meter strip
     *                  
     * Input          : pointer to ROM pattern; pattern length; frame rate
     *                  
     * Output         : None
     * Return         : None
     *******************************************************************************/
    void send_1M_pattern(const unsigned long data[][10], int pattern_no, int frame_rate)
    
    
    {
      int i=0;
      int j=0;
      uint32_t temp_data;
    
    
      for (i=0;i<pattern_no;i++)
      {
        noInterrupts();
        for (j=0;j<10;j++)
        {
          // Convert Hex to seperate RGB Values
         long r=(long)(temp_data>>16);
         long g=(long)(r>>8);
         long b=(long)temp_data;
    
        // Apply multiplication factor for brightness
        r = (float)r * (a_val/1024.0);
        g = (float)g * (a_val/1024.0);
        b = (float)b * (a_val/1024.0);
    
    // Convert RGB values back to Hex
    long temp_data = ((long)r << 16) | ((long)g << 8 ) | (long)b;
          temp_data=pgm_read_dword_near(&data[i][j]);
          send_strip(temp_data);
        }
        interrupts();
    
    
        delay(frame_rate);
    
    
      }

     

    I wasn't sure where exactly to put it but when I did what you said to do I got this error.

     

    "Tri_Strip_Brightness.ino: In function 'void send_1M_pattern(const long unsigned int (*)[10], int, int)':

    Tri_Strip_Brightness:226: error: 'a_val' was not declared in this scope"

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gadget.iom
    gadget.iom over 12 years ago in reply to josh_j

    Try moving the line "temp_data=pgm_read_dword_near(&data[i][j]);" above the code I sent you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gadget.iom
    gadget.iom over 12 years ago in reply to josh_j

    Try moving the line "temp_data=pgm_read_dword_near(&data[i][j]);" above the code I sent you.