Arduino
  • Products
  • More
Arduino
Arduino Forum Who wants RadioBlocks (Simple Radio for Arduino)?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 420 subscribers
  • Views 1813 views
  • Users 0 members are here
Related

Who wants RadioBlocks (Simple Radio for Arduino)?

fustini
fustini over 12 years ago

Back in June, I met Colorado Micro Devices at the Sensors Expo in Chicago.   I posted about their RadioBlock modules on here on element14:

  • Re: Arduino drop-in IEEE 802.15.4 radio module
  • RadioBlocks: drop-in IEEE 802.15.4 wireless module for Raspberry Pi

 

They also kindly gave me some modules to try out:

image

RadioBlocks | Colorado Micro Devices

"Simple Radio for Arduino or any Embedded System"

The Colorado Micro Devices RadioBlock is an IEEE 802.15.4 FCC and CE certified wireless modem. It has a simple UART interface to make it easy to drop into your end product or to experiment with. A standard 100 mil pin spaced header means you can plug it right into many common boards: Arduino, Raspberry Pi, BeagleBone, it’s easy – No special pin configuration or adapter board needed! If you can connect RXd, TXd, Power and GND, you are ready to unplug and go wireless. It has an onboard regulator so it is 5V tolerant for boards with 5V IO. To make it even easier we’ve written a simple wireless mesh network we call SimpleMesh. SimpleMesh automatically routes your data to the node you address and we’ve created Arduino and C libraries for you so you can spend your time on your app and not on networking. Since these stacks are open source you don’t need anyone’s permission to to hack them.

image

 

I've not had time to try them out, so I thought I would pass on the favor to another member of element14 Community:

 

  • 2x RadioBlock "Mains" Powered: http://www.coloradomicrodevices.com/shop/radio-block/

image

  • 1x RadioBlock Battery Powered: RadioBlock | Colorado Micro Devices

image

  • 2x USB2UART: http://www.coloradomicrodevices.com/shop/usb2uart/

image

  • 1x Adapter board: JTAG/ISP Board | Colorado Micro Devices

image

  • 1x Connector Kit: RadioBlock Connector Kit | Colorado Micro Devices


I'm going to ship all of of these modules for free it to one lucky Community member (sorry, no minors, you must be 18 years of age or older):


  • Reply to this post with a short description of why you are interested (1 to 2 sentences is fine)
  • I'll will pick a winner at random on Monday, December 2nd, at 5pm US CDT.

 

Note: I'm located in Chicago and will ship it for free to the winner using the lowest cost option available.  If the winner is located outside the US, then the winner will be responsible for paying any customs fees or duty that may apply.  I will list the value as $121 USD.

 

Cheers,

Drew

http://twitter.com/pdp7

  • Sign in to reply
  • Cancel

Top Replies

  • bltsandwich1
    bltsandwich1 over 12 years ago +1
    I would love to try these out, and make a few videos about them! Really interesting to see such small devices, and there is a ton that I can see being done with these! As always, Thanks Drew!
  • digitalman2112
    digitalman2112 over 12 years ago +1
    The crew at FamiLAB would love to try them out - we've been wanting to setup some nodes to monitor environmental status, tool status, etc - these would be a great start!
  • arturcieslak1
    arturcieslak1 over 12 years ago +1
    It would be great to use RadioBlock with Arduino Uno (thanks Drew) or chipKIT Max32 (thank again, Drew) to build communication system for the robot on which I'm currently working (more info soon).
Parents
  • fustini
    fustini over 12 years ago

    I took alpha sorted list of names:

    image

    and took the first place after a random sort as the winner:

    image

    Congrats to kas.lewis!

     

    Kas: please add me as Contact and send a private message with your shipping address.

     

    cheers,

    drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • fustini
    fustini over 12 years ago

    I took alpha sorted list of names:

    image

    and took the first place after a random sort as the winner:

    image

    Congrats to kas.lewis!

     

    Kas: please add me as Contact and send a private message with your shipping address.

     

    cheers,

    drew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • kas.lewis
    kas.lewis over 12 years ago in reply to fustini

    Hello Drew,

     

    Thank you very much for these modules and for the opportunity to play around with them. I hope to put them to good use and hopefully let you know how it worked and if it worked for my project.

     

    Thankfully

    Kas

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to kas.lewis

    Hey does anyone know the updated scoop with these little devices and or coloradomicrodevices - the shopping page on their website is gone as are the forums.  It seems like these devices are really relevant so maybe the company has been acquired?  Anyway, I'd like to get my hands on a few of these if I can figure out where...