Arduino
  • Products
  • More
Arduino
Arduino Forum LCD On/Off
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 415 subscribers
  • Views 170 views
  • Users 0 members are here
Related

LCD On/Off

hobbit666
hobbit666 over 12 years ago

I have a cheap 128x64 graphic lcd (12864ZW) and got it all working etc.

 

I'm trying to do a small project that when a push switch (may change to proximity sensor) is pressed the LCD displays some messages/graphics etc. then clears until activated again.  As i'm doing as a standalone project and want to save battery (going to use a 9V battery) can I just plug the +5V into a pin on the Arduino and when the switch is pressed make that pin on to supply the +V to the screen?

 

Or will I need to do this with a relay of some sort?

 

Going to do a blog on my project but need some pointers on getting the breadboard prototype to work.

  • Sign in to reply
  • Cancel
Parents
  • gadget.iom
    gadget.iom over 12 years ago

    Hi Neil

    According to the datasheet for your LCD, the maximum current consumption is 45mA. The most that an Arduino pin is rated for is about 40mA, though 20mA is the maximum recommended current for long duty cycles.

    You should be able to switch the LCD through a transistor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gadget.iom
    gadget.iom over 12 years ago

    Hi Neil

    According to the datasheet for your LCD, the maximum current consumption is 45mA. The most that an Arduino pin is rated for is about 40mA, though 20mA is the maximum recommended current for long duty cycles.

    You should be able to switch the LCD through a transistor.