Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Toner Transfer method for inkjet printers?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 419 subscribers
  • Views 8489 views
  • Users 0 members are here
  • toner
  • pcb
  • make
  • diy
  • transfer
Related

Toner Transfer method for inkjet printers?

RobPaige
RobPaige over 12 years ago

So I spent a rather fruitless Monday printing, ironing, cleaning, repeating, all in a bid to get the toner transfer method to work. I used an HP 7520, printing on photo paper, advertising circulars, and regular 20 pound bond printer paper, (using both the photo paper tray, which prints in phto ink, and the main tray).and could not get it to work. I've heard that overhead transparency sheets will do the trick, but before I spend a fortune on those, I though I'd solicit your advice.

  • Sign in to reply
  • Cancel

Top Replies

  • billpenner
    billpenner over 12 years ago +2
    Typically the transfer method requires a Laser print. Ink jet printers use ink which soaks into the paper while Laser printers use a plastic powder (toner) which is melted onto the paper/transparency which…
  • shabaz
    shabaz over 12 years ago +2
    Rob Paige wrote: I've heard that overhead transparency sheets will do the trick, but before I spend a fortune on those, I though I'd solicit your advice. It's all about how dense you can get the…
  • ntewinkel
    ntewinkel over 12 years ago in reply to billpenner +1
    I haven't tried it myself, but from what I've seen the "toner" part of "toner transfer" refers to the toner in a laser printer. But don't photocopiers use laser/toner? So a 3 cent copy at a place like…
Parents
  • shabaz
    shabaz over 12 years ago

    Rob Paige wrote:

     

    I've heard that overhead transparency sheets will do the trick, but before I spend a fortune on those, I though I'd solicit your advice.

    It's all about how dense you can get the print, and that likely varies from printer to printer, and type of acetate sheet (some sheets melt in the photocopier : ) From what I've heard, apparently older printers/copiers may be better at it.

    If you can hold the printed sheet it to the light and barely see anything through the toner, then that is likely to work. Otherwise, it is not worth going ahead with the rest of the process.

    I used to do this for some boards, and then later discovered a company that did photoplotting (which is the ultimate in density) but now I don't do that either, because the photoplotting service is still relatively expensive : (

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • RobPaige
    RobPaige over 12 years ago in reply to shabaz

    Just out of curiosity, what do you use these days?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • RobPaige
    RobPaige over 12 years ago in reply to shabaz

    Just out of curiosity, what do you use these days?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 12 years ago in reply to RobPaige

    Hi Rob,

    After it got too expensive with photoplots (and I didn't have a decent laser printer), I just use a local firm to create the board from the CAD files, or alternatively there are some companies in China too, for lower cost. However there is the delay, so it's not really a solution :-(, just an option of working around if you are willing to tolerate a delay of a couple of weeks. I think I would re-try a home method at some stage, but I need to re-obtain chemicals, heater, bath, etc - not sure I still have them :-( although I kept the home-made UV source (nothing sophisticated, a few UV tubes placed inside a flatbed scanner case, with normal fluorescent tubes interspersed and a switch, so it can double as a normal light box).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • vsluiter
    vsluiter over 12 years ago in reply to RobPaige

    For prototypes I use either iteadstudio, and with $25 shipment you'll get your boards within 3 weeks. The other option I use is Wuerth Elektronik. More expensive, but more consistent in quality.