Arduino
  • Products
  • More
Arduino
Arduino Forum Arduinio Drucksensor
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 418 subscribers
  • Views 998 views
  • Users 0 members are here
  • drucksensor
Related

Arduinio Drucksensor

e14 Contributor
e14 Contributor over 12 years ago

Hallo liebe USER,

 

ich bin Student und zur Zeit belege ich ein Projekt, in dem man einen Testprüfstand für eine Modellgasturbine bauen soll. Meine Aufgabe ist es, mit Hilfe von Arduino an mehreren Stellen Druck Temperatur und Durchfluss zu messen. Ich habe bereits einen Druck und Temperartursensor angeschlossen und diese erfassen auch Daten. Jedoch ist der jetzige Sensor nicht für die vorliegenden Drücke ausgelegt. Mein Frage ist nun, ob mir jemand von euch einen Drucksensor für den Arduino Uno vorschlagen kann, welcher Drücke bis zu 5 bar messen kann!!! Dazu wäre es hilfreich wenn es vielleicht sogar ein schon vorhandenes Programm dazu geben würde.

 

Wenn jemand eine Lösung oder einen Vorschlag hätte wäre ich sehr dankbar.

 

MFG Thomas

 

PS: Bin erst seit gerade Mitglied in diesem Forum

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago

    Considering your trying to measure 5Bar, you will want a transducer that goes above that for safety and for ensuring you don't saturate the readings

     

    these are a few available directly from Newark (Element14) that should satisfy your needs, some of them provide a voltage output that could be directly read by the arduino or pre-processed by a voltage divider or amplifier

     

    http://canada.newark.com/webapp/wcs/stores/servlet/Search?catalogId=15003&langId=1&storeId=10196&categoryId=800000005754&st=pressure%20aensor&pageSize=25&showResults=true&sf=422&pf=810042608

     

    a point to note is SAFETY. when measuring GAS (Explosive mixtures) it is critical that the transducers are rated for this use and of course with any temperature extremes that may be present. In the gas industry (In the UK) this is often referred to as Intrinsically Safe Devices where power is limited out to the measuring device in order to minimize the chances of an explosion should GAS and a spark occur in the same place. One popular techniques is to use 4-20mA loops with isolation barriers in-between the controller and the transducer. (Beyond the scope of this discussion, but loads of information on the WEB)

     

    with voltage or current devices it is a simple matter to read the values with the analog inputs of the arduino, possibly with suitable pre processing for current to volts for example, there are loads of example code for reading the analog inputs on the atmel devices.

     

    Be careful !!! and good luck

     

    regards

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to Robert Peter Oakes

    Hallo Peter,thank you for your quick response.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to e14 Contributor

    more than welcome, I hope it helps and good luck

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to Robert Peter Oakes

    Hello Peter,

    furthermore i need to install an air flow rate sensor, but i only find a sensor for water, fuel and so on and not for air.

    Could you help me?

    Thank you in advance

     

    Thomas

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to e14 Contributor

    ebay has quite a selection

    http://www.ebay.com/sch/Business-Industrial-/12576/i.html?_from=R40&_sac=1&_nkw=air+flow+sensor

     

    also this may shed more light on the subject http://www.flowmeters.com/

     

    from my quick checks, ebay may be your best bet, you will however need to create code and or circuitry to convert it to a signal able to be read /used by the Arduino

     

    depending on what you choose.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • guidoeagle
    guidoeagle over 12 years ago in reply to e14 Contributor

    Hallo Thomas,

     

    Luftmassenmesser LMM (mass air flow meter) werden auch bei Verbrennungsmotoren eingesetzt. Siehe z. B. "File:Caucho.jpg - Wikimedia Commons" aus dem Artikel "Luftmassenmesser – Wikipedia". Das Auslesen diese LMMs ist nicht besonders schwer. Wenn ich mich richtig erinnere benötigt man lediglich eine genaue Spannungsversorgung und einen AD-Wandler. Neuer LMMs geben angeblich sogar schon digitale Messwerte aus.


    Mit freundlichen Grüßen

    Guido

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • guidoeagle
    guidoeagle over 12 years ago in reply to e14 Contributor

    Hallo Thomas,

     

    Luftmassenmesser LMM (mass air flow meter) werden auch bei Verbrennungsmotoren eingesetzt. Siehe z. B. "File:Caucho.jpg - Wikimedia Commons" aus dem Artikel "Luftmassenmesser – Wikipedia". Das Auslesen diese LMMs ist nicht besonders schwer. Wenn ich mich richtig erinnere benötigt man lediglich eine genaue Spannungsversorgung und einen AD-Wandler. Neuer LMMs geben angeblich sogar schon digitale Messwerte aus.


    Mit freundlichen Grüßen

    Guido