Arduino
  • Products
  • More
Arduino
Arduino Forum hi guys i have problem with program
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 417 subscribers
  • Views 1157 views
  • Users 0 members are here
Related

hi guys i have problem with program

e14 Contributor
e14 Contributor over 12 years ago

i am  working on project .

 

i have two sensor "button 1" and "button".when button 1 will activate it will turn on led1 for 1000 mili seconds and led 2 will be off during this.

and if button 2 activate it will turn on led 2 for 1000 msec and led1 will be off for same time.

 

i am having the error"   button state2 was not declared in this scope highlight on the this line   "  buttonState1 = digitalRead(buttonPin1);"

 

const int buttonPin1 = 2;     // the number of the pushbutton pin 2

const int buttonPin2 = 3;     // the number of the pushbutton pin 3

const int ledPin1 =  13;      // the number of the LED pin

const int ledPin2 =  12;

// variables will change:

int buttonState = 0;         // variable for reading the pushbutton status

 

 

void setup() {

  // initialize the LED pin as an output:

  pinMode(ledPin1, OUTPUT);   

  pinMode(ledPin2, OUTPUT); 

  // initialize the pushbutton pin as an input:

  pinMode(buttonPin1, INPUT);

  // initialize the pushbutton pin as an input:

  pinMode(buttonPin2, INPUT);   

}

 

 

void loop(){

  // read the state of the pushbutton value:

  buttonState1 = digitalRead(buttonPin1);

  // read the state of the pushbutton value:

  buttonState2= digitalRead(buttonPin2);

 

 

  // check if the pushbutton is pressed.

  // if it is, the buttonState is HIGH:

  if (buttonState1 == HIGH) {    

    // turn LED on:   

    digitalWrite(ledPin1, HIGH); 

    delay(1000);

    digitalWrite(ledPin2, LOW);

    delay(1000);

  if

     (buttonState2 == HIGH) {    

    // turn LED on:   

    digitalWrite(ledPin2, HIGH); 

    delay(1000);

    digitalWrite(ledPin1, LOW);

    delay(1000);

  }

  }

 

  

}

Attachments:
sketch_may13e.ino.zip
  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to gihu +1
    Thanks a million giu.
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to gihu +1
    it worked thanks
  • gihu
    gihu over 12 years ago

    Hi Omair,

     

    You are creating just one variable 'int buttonState', but you never use it. Instead of using it you are trying to use buttonState1 and buttonState2, that you do not have declared before.

    Try

    // variables will change:

    int buttonState1 = 0;         // variable for reading the first pushbutton status

    int buttonState2 = 0;         // variable for reading the second pushbutton status

     

    Hope that helps,

    Miguel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to gihu

    Thanks a million giu.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • gihu
    gihu over 12 years ago in reply to e14 Contributor

    Did it work?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to gihu

    it worked thanks