Arduino
  • Products
  • More
Arduino
Arduino Forum Adding wifi to control a uno basic motor driven robot
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 418 subscribers
  • Views 963 views
  • Users 0 members are here
  • wifi
  • joystick
  • arduino
Related

Adding wifi to control a uno basic motor driven robot

e14 Contributor
e14 Contributor over 12 years ago

I have a uno with an dual hbridge motor controller and two motors

attached to a uno

i was thinking of adding wifi to allow me to drive the robot from an app or a joystick

 

Any advice on how start ? 

 

Thanks

  • Sign in to reply
  • Cancel
Parents
  • dougw
    dougw over 12 years ago

    You can get a WiFi module for your arduino, but it is cheaper to get a Bluetooth module such as an HC-05 with carrier card to make connection easy. This could be controlled from a smart phone or a PC.

    Arduino Tutorial #8 - Controlling Robots with Bluetooth (HC-05) - YouTube

    Arduino AND Bluetooth HC-05 Connecting easily

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to dougw

    I heard blue tooth has limited distance and drops off all the time

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shtuk41
    shtuk41 over 12 years ago in reply to e14 Contributor

    Dropping connection can be annoying....But I like the idea of getting control with a smart phone!  Xbee worked perfect for me inside the house, but it also dropped the connection outside, so I guess you would have to include a connection recovery in your design with either technology ....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 12 years ago in reply to e14 Contributor

    I use an HC-05 which is Bluetooth class 2 (30 meters) connected to my Galaxy Note and it works well throughout my 2-story house, including through walls. If you want better range you can get a Bluetooth class 1 device (100 m).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 12 years ago in reply to e14 Contributor

    I use an HC-05 which is Bluetooth class 2 (30 meters) connected to my Galaxy Note and it works well throughout my 2-story house, including through walls. If you want better range you can get a Bluetooth class 1 device (100 m).