Arduino
  • Products
  • More
Arduino
Arduino Forum Using MIT App Inventor to create Android Apps which can connect to Arduino via Bluetooth
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 415 subscribers
  • Views 493 views
  • Users 0 members are here
  • android
  • mit
  • appinventor
  • arduino
Related

Using MIT App Inventor to create Android Apps which can connect to Arduino via Bluetooth

neilk
neilk over 12 years ago

I was enthused by Pieter Bok’s recent post  involving an iPhone App connecting to an Arduino via WiFi:


http://www.element14.com/community/videos/12327/l/arduino-based-automatic-irrigation-system-for-pot-plants


I don’t have an iPhone, or a WiFi shield, but Bluetooth was mentioned in the thread,  so I Googled around for Android, Arduino and Bluetooth, finding several links which made use of an amazing, FREE resource from MIT called App Inventor, for developing Android Apps:


http://appinventor.mit.edu/explore


This link is to version 2 of App inventor. Several of the Arduino related links, were for App Inventor version 1, which is still available, although not for long, so you are advised not to start using it.


App Inventor 2 is entirely web-based, and includes the ability to connect to your target Android device via Wifi and run an emulation of your App in real time - the display on your device changes as you change the design in App Inventor! If you don’t even have an Android device, you can run an emulator on your PC and App Inventor will connect to it.


App Inventor 2 has two screens - Design and Blocks. In Design, you drag and drop components such as buttons, labels, text boxes, sliders, etc, on to a representation of your Android device screen and arrange them as you want them to appear.


In the Blocks screen, you drag and drop representations of code segments which relate the display components together and ultimately generate your app. Once you get into it, it’s actually very straightforward.


I've posted my initial experiences of using App Inventor on my Blog:

 

http://www.element14.com/community/people/neilk/blog/2014/07/14/mit-app-inventor-creating-android-app-to-control-arduino-via-bluetooth

 

I intend to post more, so if you are interested, please keep a look out.

 

Neil

  • Sign in to reply
  • Cancel
  • neilk
    neilk over 11 years ago

    Hi everyone and apologies - I spotted a stupid error in the first App Inventor block in this Blog post.


    I have corrected the post and the title now includes the fact that it has been corrected. The original link still works.

     

    Neil