I built most of this circuit, but before I finished it I connected the motor to just one tip125 then to the tip120 on the other side
of the bridge. I was glad I did because I could never get the tip120 to turn off. It is an H-bridge that is controlled by
(hopefully) an arduino. I am hoping to use an op amp to amp the voltage from the arduino to then control the two 2n4403
transistors. My problem is the signal from the small 2n4403 to the h-bridge transistors never goes to ground. I tried controlling
it with potentiometers and whatever I tried I could not turn off the tip120 s with the 2n4403. I can control the tip125 s well enough
but that doesn't make a working h-bridge. Any help with this would be appreciated.
schematic made with easyeda.com software