Arduino
  • Products
  • More
Arduino
Arduino Forum Measure square wave frequency
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 421 subscribers
  • Views 5593 views
  • Users 0 members are here
  • square
  • arduino
  • frequency
Related

Measure square wave frequency

e14 Contributor
e14 Contributor over 12 years ago

Hello,

 

I'm working with the Arduino Due ans I used the following code:

 

// period of pulse accumulation and serial output, milliseconds

#define MainPeriod 100

long previousMillis = 0; // will store last time of the cycle end

volatile unsigned long duration=0; // accumulates pulse width

volatile unsigned int pulsecount=0;

volatile unsigned long previousMicros=0;

 

void setup()

{

  Serial.begin(19200);

  attachInterrupt(6, myinthandler, RISING);

}

 

void loop()

{

  unsigned long currentMillis = millis();

  if (currentMillis - previousMillis >= MainPeriod)

  {

    previousMillis = currentMillis;  

    // need to bufferize to avoid glitches

    unsigned long _duration = duration;

    unsigned long _pulsecount = pulsecount;

    duration = 0; // clear counters

    pulsecount = 0;

    float Freq = 1e6 / float(_duration);

    Freq *= _pulsecount; // calculate F

    // output time and frequency data to RS232

    Serial.print(currentMillis);

    Serial.print(" "); // separator!

    Serial.print(Freq);

    Serial.print(" ");

    Serial.print(_pulsecount);

    Serial.print(" ");

    Serial.println(_duration);

  }

}

 

void myinthandler() // interrupt handler

{

  unsigned long currentMicros = micros();

  duration += currentMicros - previousMicros;

  previousMicros = currentMicros;

  pulsecount++;

}

 

to measure the frequency.

 

I can measure frequencies higher than 1.5kHz accurately, but I can't seem to measure lower frequencies.

 

How can I measure lower frequencies, say 400Hz and above?

 

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 12 years ago +1
    Hi Matt, I don't know about this situation but usually sampling over a longer time period will improve accuracy. John
  • D_Hersey
    D_Hersey over 12 years ago in reply to jw0752 +1
    John is right, there I said it! You might be able to get more accurate timing by latching the wdt upon interrupt. Reset the Arduino Due board using the watchdog - Arduino Forum
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to D_Hersey +1
    I tried setting mainPeriod to be longer but it still didn't measure accurately lower frequencies. Regarding the wdt , I don't understand how can it help, can you elaborate? thanks.
Parents
  • ravi_butani
    ravi_butani over 12 years ago

    // mills() reference http://arduino.cc/en/Reference/millis
    // attachinterrupt() reference http://arduino.cc/en/Reference/attachInterrupt
    // Due pin 0,1,2 corresponding to pin interrupt 0,1,2 respectively
    // All the best from RAVI BUTANI
    // this code measures frequency only accurate for >100Hz
    // for less frequency minor modifications needed
    
    
    unsigned long time_stamp;
    unsigned int count0 = 0;
    unsigned int count1 = 0;
    unsigned int count2 = 0;
    
    
    unsigned int output0 = 0;
    unsigned int output1 = 0;
    unsigned int output2 = 0;
    
    
    void setup()
    {
      Serial.begin(9600);
      time_stamp = millis();
      attachInterrupt(0, sensor0, RISING); // sensor 1 on mega pin no 2 Due pin 0
      attachInterrupt(1, sensor1, RISING); // sensor 2 on mega pin no 3 Due Pin 1
      attachInterrupt(2, sensor2, RISING); // sensor 3 on mega pin no 21 Due Pin 2
    }
    
    
    void loop()
    {
      if(millis() - time_stamp > 50)
      {
        detachInterrupt(0); // disable interrups
        detachInterrupt(1);
        detachInterrupt(2);
        output0 = count0 * 20;
        output1 = count1 * 20;
        output2 = count2 * 20;
        Serial.print("Sensor0 Reading = ");
        Serial.println(output0);
        Serial.print("Sensor1 Reading = ");
        Serial.println(output1);
        Serial.print("Sensor2 Reading = ");
        Serial.println(output2);
        delay(40);
        count0 = 0;
        count1 = 0;
        count2 = 0;
        time_stamp = millis();
        attachInterrupt(0, sensor0, RISING); // we have done with this mesasurenment,enable interrups for next cycle
        attachInterrupt(1, sensor1, RISING);
        attachInterrupt(2, sensor2, RISING);
      }
    }
    
    
    void sensor0()
    {
      count0++;
    }
    
    
    void sensor1()
    {
      count1++;
    }
    
    
    void sensor2()
    {
      count2++;
    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to ravi_butani

    Thanks for your reply.

     

    I tried that, it measures 1500Hz and higher quite accurately but anything below it and it fails.

     

    Do you know what else can be done to fix this?

     

    Thanks again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to e14 Contributor

    So in short, yes you can do it, I have done it before, a while back. I wont be able to investigate until the weekend though

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ravi_butani
    ravi_butani over 12 years ago in reply to e14 Contributor

    Hey Matt, its obvious that if you want to measure low freq accurately you need long time window ...means your measurement time increases... in my code i hv kept time window of 50ms...

    you can consider more time window for accurate low freq measurements..

    modify these lines..

    if(millis() - time_stamp > 50)// 50ms window

    output0 = count0 * 20;

    all three outputx lines

     

    to

    if(millis() - time_stamp > 500)// 500ms window

    output0 = count0 * 2;

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to ravi_butani

    I'll try that later and report back, thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to ravi_butani

    Thanks! It works.

     

    Can you please elaborate on how it works, I don't fully understand. thank you.

     

    Also, there is a problem that there is a small deviation of 2-5Hz in the reading and it takes about 3-4 seconds to get the accurate reading.

     

    Can it get more accurate with better resolution?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ravi_butani
    ravi_butani over 12 years ago in reply to e14 Contributor

    do same thing with this code for getting more accurate readings...obviously it takes some more time...

    if(millis() - time_stamp > 1000)// 1sec window

    output0 = count0;

    elaboration..

    There are two ways to measure frequency..

    1. measure time period of signal by taking mcu clock as reference... example is your code with timer library   code uses hardware timer its much accurate but for multiple input signal multiple timers needed

    2. measure no of pulse in unit time .... code I have posted 

    here single hardware timer with with multiple pin interrupts used its less accurate

     

    best way is combining Hardware timer to generate accurate time window... and hardware counters for count no of pulses in this time window..

    unfortunately i havnt find any arduino contributed library for this purpose... And i havnt gone for backbone programming of atmega mcus... I can do it with msp430 bcoz I have long experience with msp430 backbone programming...

    any way I am happy that my help is useful for your project... all the best... and keep posting ur queries... we r always here to help you out..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to ravi_butani

    Thanks again, you really helped me.

     

    One last question, I understand that we count the number of pulses in a time window, what I don't understand is the multiplication in 2 of the number of pulses to get the frequency. Can you please explain that?

     

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    In ravi's example, the time window is 500 milliseconds (1/2) of a second. Since frequency is cycles per second, you multiply the number of pulses recorded in time period t by 1000 milliseconds (1 second) over time period t in milliseconds, which gives us 2.  The result is the number of pulses (cycles) in one full second, aka frequency.  It is the average frequency over that 500 millisecond time period.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to ravi_butani

    Dear Ravi Butani...

    Thanks for sharing the knowledge. I am facing the problem with measurement of square wave from freq range 100KHz to 10 MHz....

    Please explain how it is possible using Arduino Due

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 10 years ago in reply to e14 Contributor

    At some point, the 16 Mhz processor cannot run the code fast enough to respond to the frequency you are trying to measure. My guess is 10 Mhz is at that point.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to e14 Contributor

    The trick to counting high frequency signals with the Arduinos is not to, let the hardware do it using a timer counter register clocked by your signal, then what you do is read the value at a fixed interval and compare the difference, this will tell you the frequency with a little simple math

     

    Here is a library that works upto 8Mhz or so the docs say

     

    Lab3 - Laboratory for Experimental Computer Science

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to e14 Contributor

    The trick to counting high frequency signals with the Arduinos is not to, let the hardware do it using a timer counter register clocked by your signal, then what you do is read the value at a fixed interval and compare the difference, this will tell you the frequency with a little simple math

     

    Here is a library that works upto 8Mhz or so the docs say

     

    Lab3 - Laboratory for Experimental Computer Science