Arduino
  • Products
  • More
Arduino
Arduino Forum Measure square wave frequency
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 421 subscribers
  • Views 5593 views
  • Users 0 members are here
  • square
  • arduino
  • frequency
Related

Measure square wave frequency

e14 Contributor
e14 Contributor over 12 years ago

Hello,

 

I'm working with the Arduino Due ans I used the following code:

 

// period of pulse accumulation and serial output, milliseconds

#define MainPeriod 100

long previousMillis = 0; // will store last time of the cycle end

volatile unsigned long duration=0; // accumulates pulse width

volatile unsigned int pulsecount=0;

volatile unsigned long previousMicros=0;

 

void setup()

{

  Serial.begin(19200);

  attachInterrupt(6, myinthandler, RISING);

}

 

void loop()

{

  unsigned long currentMillis = millis();

  if (currentMillis - previousMillis >= MainPeriod)

  {

    previousMillis = currentMillis;  

    // need to bufferize to avoid glitches

    unsigned long _duration = duration;

    unsigned long _pulsecount = pulsecount;

    duration = 0; // clear counters

    pulsecount = 0;

    float Freq = 1e6 / float(_duration);

    Freq *= _pulsecount; // calculate F

    // output time and frequency data to RS232

    Serial.print(currentMillis);

    Serial.print(" "); // separator!

    Serial.print(Freq);

    Serial.print(" ");

    Serial.print(_pulsecount);

    Serial.print(" ");

    Serial.println(_duration);

  }

}

 

void myinthandler() // interrupt handler

{

  unsigned long currentMicros = micros();

  duration += currentMicros - previousMicros;

  previousMicros = currentMicros;

  pulsecount++;

}

 

to measure the frequency.

 

I can measure frequencies higher than 1.5kHz accurately, but I can't seem to measure lower frequencies.

 

How can I measure lower frequencies, say 400Hz and above?

 

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 12 years ago +1
    Hi Matt, I don't know about this situation but usually sampling over a longer time period will improve accuracy. John
  • D_Hersey
    D_Hersey over 12 years ago in reply to jw0752 +1
    John is right, there I said it! You might be able to get more accurate timing by latching the wdt upon interrupt. Reset the Arduino Due board using the watchdog - Arduino Forum
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to D_Hersey +1
    I tried setting mainPeriod to be longer but it still didn't measure accurately lower frequencies. Regarding the wdt , I don't understand how can it help, can you elaborate? thanks.
Parents
  • D_Hersey
    D_Hersey over 10 years ago

    Years and years ago I read a paper where they used a phase detector to charge a capacitor in proportion to the residue to get past roundoff.  This was during a period of fervid work on PLLs and FLLs.  Too sophisticated a method to use here, but there are many ways to skin a cat.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • D_Hersey
    D_Hersey over 10 years ago

    Years and years ago I read a paper where they used a phase detector to charge a capacitor in proportion to the residue to get past roundoff.  This was during a period of fervid work on PLLs and FLLs.  Too sophisticated a method to use here, but there are many ways to skin a cat.