Arduino
  • Products
  • More
Arduino
Arduino Forum Measure square wave frequency
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 421 subscribers
  • Views 5593 views
  • Users 0 members are here
  • square
  • arduino
  • frequency
Related

Measure square wave frequency

e14 Contributor
e14 Contributor over 12 years ago

Hello,

 

I'm working with the Arduino Due ans I used the following code:

 

// period of pulse accumulation and serial output, milliseconds

#define MainPeriod 100

long previousMillis = 0; // will store last time of the cycle end

volatile unsigned long duration=0; // accumulates pulse width

volatile unsigned int pulsecount=0;

volatile unsigned long previousMicros=0;

 

void setup()

{

  Serial.begin(19200);

  attachInterrupt(6, myinthandler, RISING);

}

 

void loop()

{

  unsigned long currentMillis = millis();

  if (currentMillis - previousMillis >= MainPeriod)

  {

    previousMillis = currentMillis;  

    // need to bufferize to avoid glitches

    unsigned long _duration = duration;

    unsigned long _pulsecount = pulsecount;

    duration = 0; // clear counters

    pulsecount = 0;

    float Freq = 1e6 / float(_duration);

    Freq *= _pulsecount; // calculate F

    // output time and frequency data to RS232

    Serial.print(currentMillis);

    Serial.print(" "); // separator!

    Serial.print(Freq);

    Serial.print(" ");

    Serial.print(_pulsecount);

    Serial.print(" ");

    Serial.println(_duration);

  }

}

 

void myinthandler() // interrupt handler

{

  unsigned long currentMicros = micros();

  duration += currentMicros - previousMicros;

  previousMicros = currentMicros;

  pulsecount++;

}

 

to measure the frequency.

 

I can measure frequencies higher than 1.5kHz accurately, but I can't seem to measure lower frequencies.

 

How can I measure lower frequencies, say 400Hz and above?

 

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 12 years ago +1
    Hi Matt, I don't know about this situation but usually sampling over a longer time period will improve accuracy. John
  • D_Hersey
    D_Hersey over 12 years ago in reply to jw0752 +1
    John is right, there I said it! You might be able to get more accurate timing by latching the wdt upon interrupt. Reset the Arduino Due board using the watchdog - Arduino Forum
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to D_Hersey +1
    I tried setting mainPeriod to be longer but it still didn't measure accurately lower frequencies. Regarding the wdt , I don't understand how can it help, can you elaborate? thanks.
Parents
  • michaelkellett
    michaelkellett over 10 years ago

    When you measure frequency you need to adopt different strategies if your pulse frequency is not much faster than the gate period and of course your clock frequency needs to be much higher than the pulse frequency. If you are counting input pulses per gate period then the best you can do with 1 second gate is 0.5% resolution at 200Hz.

    If you count clock pulses per input pulse then an 8MHz clock gives you 0.0025% resolution at 200Hz but only 0.05% resolution at 4kHz.

    You'll get better results if you count clock pulses per n input pulses and adjust n to keep the gate period constant, and even better results if you generate a new count after every input pulse but then calculate the frequency over the last n input pulses and average the results.

     

    The timer in the AVR offers input capture - I'm not sure which Arduino you have but if based on a atmega328 you have 16 bit resolution at  up to 16 MHz  - you will need to able to service an interrupt at the pulse frequency and read the timer capture register on each rising or falling edge. This will probably need you to code in C at register level but you should be able to measure 200Hz to 4kHz with 1part in 4 - 8million resolution over that range (using a 1 second gate time and variable n (see above)). The accuracy will depend on the accuracy of the processor clock.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 10 years ago

    When you measure frequency you need to adopt different strategies if your pulse frequency is not much faster than the gate period and of course your clock frequency needs to be much higher than the pulse frequency. If you are counting input pulses per gate period then the best you can do with 1 second gate is 0.5% resolution at 200Hz.

    If you count clock pulses per input pulse then an 8MHz clock gives you 0.0025% resolution at 200Hz but only 0.05% resolution at 4kHz.

    You'll get better results if you count clock pulses per n input pulses and adjust n to keep the gate period constant, and even better results if you generate a new count after every input pulse but then calculate the frequency over the last n input pulses and average the results.

     

    The timer in the AVR offers input capture - I'm not sure which Arduino you have but if based on a atmega328 you have 16 bit resolution at  up to 16 MHz  - you will need to able to service an interrupt at the pulse frequency and read the timer capture register on each rising or falling edge. This will probably need you to code in C at register level but you should be able to measure 200Hz to 4kHz with 1part in 4 - 8million resolution over that range (using a 1 second gate time and variable n (see above)). The accuracy will depend on the accuracy of the processor clock.

     

    MK