Arduino
  • Products
  • More
Arduino
Arduino Forum Sensor input noisy when inserted to Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 417 subscribers
  • Views 570 views
  • Users 0 members are here
  • due
  • noise
  • frequency
Related

Sensor input noisy when inserted to Arduino

e14 Contributor
e14 Contributor over 12 years ago

Hello,

 

I'm using the HB100 sensor to measure the speed of an approaching object.

 

I built amplifying and filter circuit based on the example presented here:

http://www.limpkin.fr/index.php?post/2013/08/09/Making-the-electronics-for-a-%247-USD-doppler-motion-sensor

 

After the comparator, the output is a nice square signal (images attached - yellow - signal at the IF output of the sensor, blue - signal after the amplifier and filter, purple - signal after the comparator) when the sensor detect movement.

 

I'm using the following code:

 

#define MainPeriod 10

long previousMillis = 0; // will store last time of the cycle end

volatile unsigned long duration=0; // accumulates pulse width

volatile unsigned int pulsecount=0;

volatile unsigned long previousMicros=0;

 

void setup()

{

  Serial.begin(19200);

  attachInterrupt(6, myinthandler, RISING);

}

 

void loop()

{

  unsigned long currentMillis = millis();

  if (currentMillis - previousMillis >= MainPeriod)

  {

    previousMillis = currentMillis; 

    // need to bufferize to avoid glitches

    unsigned long _duration = duration;

    unsigned long _pulsecount = pulsecount;

    duration = 0; // clear counters

    pulsecount = 0;

    float Freq = 1e6 / float(_duration);

    Freq *= _pulsecount; // calculate F

    // output time and frequency data to RS232

    Serial.print(currentMillis);

    Serial.print(" "); // separator!

    Serial.print(Freq);

    Serial.print(" ");

    Serial.print(_pulsecount);

    Serial.print(" ");

    Serial.println(_duration);

  }

}

 

void myinthandler() // interrupt handler

{

  unsigned long currentMicros = micros();

  duration += currentMicros - previousMicros;

  previousMicros = currentMicros;

  pulsecount++;

}

 

to measure the frequency. it's working for frequencies that are higher than 1.5kHz for a square wave that is generated by signal generator.

 

The problem is when I input the signal at the comparator output to pin 6 of my Arduino Due (and looking at the signals through a scope) the signals are getting very noisy, thus I can't measure the frequency accurately (when I disconnect the signal from pin 6 it all goes back to normal).

 

Any idea how to fix this?

 

Thanks.

Attachments:
image
image
  • Sign in to reply
  • Cancel
Parents
  • colin_meikle@mentor.com
    colin_meikle@mentor.com over 12 years ago

    From the scope it looks as if the pin you are connecting is configured as an output rather than an input. Have you connected it to the correct pin ? Is your attachInterrupt correct, should the first arg not be the interrupt number unless you are using Due . Most Ardiunos only have 2 external interrupts so unless you are using Due the attach doesn't look right to me i.e.

     

    Syntax

    attachInterrupt(interrupt, ISR, mode)
    attachInterrupt(pin, ISR, mode)(Arduino Due only)
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to colin_meikle@mentor.com

    I am using the Due, hence the use of attachInterrupt.

     

    In regard to the scope, all the signals in the scope images are from the sensor and the amplifying and filter circuit (see explanations in the question), not from the Arduino.

     

    because I'm using interrupts I shouldn't use pinMode(6, INPUT), should I?

     

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to colin_meikle@mentor.com

    I am using the Due, hence the use of attachInterrupt.

     

    In regard to the scope, all the signals in the scope images are from the sensor and the amplifying and filter circuit (see explanations in the question), not from the Arduino.

     

    because I'm using interrupts I shouldn't use pinMode(6, INPUT), should I?

     

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • colin_meikle@mentor.com
    colin_meikle@mentor.com over 12 years ago in reply to e14 Contributor

    Sorry Matt I missed the bit about the due, so the attachinterupt looks correct .