Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino - controlling fans and door/hatch greenhouse
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 420 subscribers
  • Views 1772 views
  • Users 0 members are here
Related

Arduino - controlling fans and door/hatch greenhouse

e14 Contributor
e14 Contributor over 12 years ago

Hi

 

I have not got a arduino yet, just checking what this thing can do for my greenhouse.

 

I want something that can do this :

 

  • Open a small door/hatch temp controlled
  • Start two fans 12v temp controlled
  • Watering system (thats for last)
  • Turn on and off heat and lights (for now this is 220v)

 

Can arduino controll 220v also? For me I've some stuff on 5-12v and 220v from my garage

 

Could anyone give a parts lits of what I need for this? Never used anything like this, except for raspberry pi, but thats not the same?

 

Frode

  • Sign in to reply
  • Cancel
Parents
  • bobcroft
    bobcroft over 12 years ago

    Frode,

              yes you can do all you want to do for your greenhouse and in fact I do all of those things in my greenhouse.  However I feel obliged to issue the usual advice regarding the 220 volt stuff, which is unless you are completely competent to work safely with such voltages you should not attempt projects involving mains electricity especially where there is likely to be water / moisture.

    At a safer level say 12 volt then you can definitely control low voltage lights, vent openers, fans and a watering system.

    For vents you need some form of motorized mechanism to move the vent, the mechanism depends on how much you need the vent to open and its weight. Alternatively a bank of low voltage fans can provide air movement.

    For my watering system I use 12 volt solenoid valves, one per plant.  Not cheap initially but very versatile.  Alternatively one valve can control several 'drippers'.

    I do use soil heating cables on my propagating benches.  These come prewired and in my case the supply cable goes into a sealed box which houses the control relay in a separate dry area.  The opto isolated control relay is controlled by an Arduino which senses temperature, humidity and ambient light level.  The DHT22 does both temperature and humidity, the BH1750 is the ambient light sensor.  The Dallas 18B20 is also an excellent temperature sensor.

    Stealing a phrase from another contributor 'Google is your friend' and my advice to you is to google each of the items you want to do and develop each aspect on its own then add it to your complete system.  All of the sensors I have mentioned have some good information on the net and often Arduino example code and libraries.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • bobcroft
    bobcroft over 12 years ago

    Frode,

              yes you can do all you want to do for your greenhouse and in fact I do all of those things in my greenhouse.  However I feel obliged to issue the usual advice regarding the 220 volt stuff, which is unless you are completely competent to work safely with such voltages you should not attempt projects involving mains electricity especially where there is likely to be water / moisture.

    At a safer level say 12 volt then you can definitely control low voltage lights, vent openers, fans and a watering system.

    For vents you need some form of motorized mechanism to move the vent, the mechanism depends on how much you need the vent to open and its weight. Alternatively a bank of low voltage fans can provide air movement.

    For my watering system I use 12 volt solenoid valves, one per plant.  Not cheap initially but very versatile.  Alternatively one valve can control several 'drippers'.

    I do use soil heating cables on my propagating benches.  These come prewired and in my case the supply cable goes into a sealed box which houses the control relay in a separate dry area.  The opto isolated control relay is controlled by an Arduino which senses temperature, humidity and ambient light level.  The DHT22 does both temperature and humidity, the BH1750 is the ambient light sensor.  The Dallas 18B20 is also an excellent temperature sensor.

    Stealing a phrase from another contributor 'Google is your friend' and my advice to you is to google each of the items you want to do and develop each aspect on its own then add it to your complete system.  All of the sensors I have mentioned have some good information on the net and often Arduino example code and libraries.