Arduino
  • Products
  • More
Arduino
Arduino Forum waveform generator with uno r3
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 421 subscribers
  • Views 3267 views
  • Users 0 members are here
  • sine
  • wave
  • arduino
  • atmel
Related

waveform generator with uno r3

e14 Contributor
e14 Contributor over 11 years ago

I have the Arduino Uno R3 and i need to generate a RF sine wave up to 500MHz.

This is not my first project with the Arduino or Atmel MCUs but it is my first RF / wave project.

 

What hardware will i need to do so?

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to shabaz +1
    Yup, I tend to agree too, it sound more achievable in a reasonable amount of time and perfect for a computer science student, not an EE. Peter
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago

    The UNO itself will not be able to help you here, it only runs at 16Mhz and even with the tightest coding will probably not exceed few Mhz on any of its pins

     

     

     

    Getting a sine wave at upto 500Mhz will require external help where the UNO would only be a controller, not the actual generator

     

     

     

    Do you have a lower frequency limit, if you generate a square wave and use external RC/LC filtering, you could approximate the sine wave

     

     

     

    What control do you want over it or is it just a static signal

     

     

     

    Basically, tell us what you intend to do with it and more about how you intend the project to function… SPECS ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to Robert Peter Oakes

    The lower limit would be about 1MHz, for my assignment, i need to create a sine wave from 1MHz to 500MHz tunable using a potentiometer or a variable in the code.

    Yes i intend for the UNO to be the controller so i want to know what external hardware do i need.

    I also know i can use a square wave instead, but if i have no limits on what hardware i can use, how would i go about doing the same without a square wave.

     

    Basically, i select a frequency, and that wave is generated. So is that static? As for any more specs, that is all i was given by my professor.

    I am actually a major in computer science and this is my first project that involves components of computer engineering.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to Robert Peter Oakes

    Oh, after hearing how ridiculous it sounded, i went back to check the project requirements..and realised i read the upper limit wrongly. (probably too tired)

     

    Anyway the actual frequency needed is 1-20 MHz in 0.1 Hz increments.

    As for amplitude it's not stated, i will ask my prof and see what he says.

     

    sorry for the confusion with the extremely high frequencies.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelwylie
    michaelwylie over 11 years ago in reply to e14 Contributor

    That's much more manageable.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelwylie
    michaelwylie over 11 years ago in reply to e14 Contributor

    If you're looking for a complete custom solution:

    http://datasheets.maximintegrated.com/en/ds/MAX038.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to michaelwylie

    that's just what i was looking for. thanks alot man.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelwylie
    michaelwylie over 11 years ago in reply to e14 Contributor

    Hope it all works out for you. That one comes in DIP so you should be able to make your circuit in perf board (vero board).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to michaelwylie

    i tried to order the max038CPP from element14, mouser, digikey but all state it as obsolete.

    is there any other IC i may use?

     

    preferably a link to a element14 product.

     

    thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelwylie
    michaelwylie over 11 years ago in reply to e14 Contributor

    Not as fancy, but should get the job done. You can order samples from Linear

    http://www.linear.com/product/LTC1799

     

    Edit: Wait! It's a square wave output. Unless you want to filter, we'll have to find another chip.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to michaelwylie

    There are DDS chips by Analog Devices, that will output a sine wave, but I'm not sure this is what his prof wants either. I think you may be right, it could have been a sig-gen controlled by GPIB etc.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to shabaz

    Yup, I tend to agree too, it sound more achievable in a reasonable amount of time and perfect for a computer science student, not an EE.

     

     

     

    Peter

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 11 years ago in reply to Robert Peter Oakes

    Lots of people (including Analog Devices) sell Analog Devices DDS chips on little boards ready for some external control.

     

    This was the first one I found (I have never dealt with these people so do some checking and look at other sources):

    AD9850 DDS Signal Generator Module 0 40MHz New | eBay

     

    I suggest the OP looks for others and also at AD's data on the chip.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 11 years ago in reply to Robert Peter Oakes

    Lots of people (including Analog Devices) sell Analog Devices DDS chips on little boards ready for some external control.

     

    This was the first one I found (I have never dealt with these people so do some checking and look at other sources):

    AD9850 DDS Signal Generator Module 0 40MHz New | eBay

     

    I suggest the OP looks for others and also at AD's data on the chip.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to michaelkellett

    Finally found out what he wants.

    He is trying to find out the effects of frequency with respect to our indoor positioning system.

    My scope is to find a device that can output 1-20 MHz and for each frequency, record the readings from the RF receivers and plot it on a graph, which we will datamine.

    So you are right, it was a sig gen controlled by GPIO.

     

    Both of us are CS people and not EE so we will just follow the advice given here. He will order the AD9850 and we will see if it works.

     

    Thanks once again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bobcroft
    bobcroft over 11 years ago in reply to e14 Contributor

    Jeremy,

                   I have used the AD 9850, others have suggested, along with an Arduino R3.  It worked without any problems using some code I found on the net, suitably modified for my needs.   There is code for a sweep generator along with AD9850.cpp and AD9850.h files on the net.  I think these will give you a basis for the frequency generator you require.  The sine waves generated at the frequencies you are interested in are good.

     

    Bob