Arduino
  • Products
  • More
Arduino
Arduino Forum waveform generator with uno r3
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 421 subscribers
  • Views 3281 views
  • Users 0 members are here
  • sine
  • wave
  • arduino
  • atmel
Related

waveform generator with uno r3

e14 Contributor
e14 Contributor over 11 years ago

I have the Arduino Uno R3 and i need to generate a RF sine wave up to 500MHz.

This is not my first project with the Arduino or Atmel MCUs but it is my first RF / wave project.

 

What hardware will i need to do so?

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to shabaz +1
    Yup, I tend to agree too, it sound more achievable in a reasonable amount of time and perfect for a computer science student, not an EE. Peter
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago

    The UNO itself will not be able to help you here, it only runs at 16Mhz and even with the tightest coding will probably not exceed few Mhz on any of its pins

     

     

     

    Getting a sine wave at upto 500Mhz will require external help where the UNO would only be a controller, not the actual generator

     

     

     

    Do you have a lower frequency limit, if you generate a square wave and use external RC/LC filtering, you could approximate the sine wave

     

     

     

    What control do you want over it or is it just a static signal

     

     

     

    Basically, tell us what you intend to do with it and more about how you intend the project to function… SPECS ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to Robert Peter Oakes

    The lower limit would be about 1MHz, for my assignment, i need to create a sine wave from 1MHz to 500MHz tunable using a potentiometer or a variable in the code.

    Yes i intend for the UNO to be the controller so i want to know what external hardware do i need.

    I also know i can use a square wave instead, but if i have no limits on what hardware i can use, how would i go about doing the same without a square wave.

     

    Basically, i select a frequency, and that wave is generated. So is that static? As for any more specs, that is all i was given by my professor.

    I am actually a major in computer science and this is my first project that involves components of computer engineering.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to e14 Contributor

    I can't see what you're professor is getting at. The span is so high, this would be a very large project containing banks of oscillators (google for oscillator circuits) but it would be very primitive, not very useful. And at 500MHz you'd need some RF experience which your professor ought to know you may not have.

    There are other methods but they are quite advanced too (would need an electrical engineering degree of some sort).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to shabaz

    Actually, im not sure what he wants too. All i know is that i am working on a small section of the project. My part is mainly software in terms of DSP and data analysis. But for this i need a POC which requires a pure wave.

    He knows that i do not have that knowledge, but my university believes strongly in self learning. As such i am given extra time to learn prior knowledge first. Any advice on what direction to go would be great.

     

    Getting equipment is not a problem for me, everything is within the school or can be claimed from them.

     

    So in this case, what would i need, say for a higher limit of maybe 200MHz?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    Do you have the equipment to measure up to 500Mhz and look at the signal to validate its integrity (I don’t for sure), maybe at the school / UNI EE Lab

     

     

     

    A 1Ghz scope would be nice, and a frequency counter. RF is such a fun subject but one I have not delved into too much so far

     

     

     

    If it where me then I would be looking at voltage controlled oscillator and perhaps a Phased locked loop (PLL) to up the frequency to the range desired

     

     

     

    There are other qualified folks looking at this in the forums too that have way more RF skills than I poses so let’s see if they can provide better suggestions

     

     

     

    Regards

     

     

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    Do you have the equipment to measure up to 500Mhz and look at the signal to validate its integrity (I don’t for sure), maybe at the school / UNI EE Lab

     

     

     

    A 1Ghz scope would be nice, and a frequency counter. RF is such a fun subject but one I have not delved into too much so far

     

     

     

    If it where me then I would be looking at voltage controlled oscillator and perhaps a Phased locked loop (PLL) to up the frequency to the range desired

     

     

     

    There are other qualified folks looking at this in the forums too that have way more RF skills than I poses so let’s see if they can provide better suggestions

     

     

     

    Regards

     

     

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to Robert Peter Oakes

    Well, i know some labs in my school that have the MSO/DPO5000B Mixed Signal Oscilloscope which can be accurate up to 2GHz and 10 GS/s maximum sampling rate.

     

    So i think it should be fine. Thanks for the direction, i shall research using VCO and PLL and perhaps wait for more folks to reply.

     

    Cheers