Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino - Ethernet module pin out, diffent model/renamed pins ? (missing SI pin)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 417 subscribers
  • Views 929 views
  • Users 0 members are here
  • hanrun
  • ethernet
  • hr911105a
  • arduino
Related

Arduino - Ethernet module pin out, diffent model/renamed pins ? (missing SI pin)

e14 Contributor
e14 Contributor over 11 years ago

image

This module has 6 pins.

 

I should only be using a few of them,,,  mainly

 

5v - GND - CS - SCK - SI and SO, and possible RST to GND

 

That's atleast what the guides say, however this module is missing the SI,

ofcourse i know it's there, but it's running under a different name, but which ?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    I think i got it,   the SI replacement is actually ST,,  not sure what the T represents... 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 11 years ago

    I think i got it,   the SI replacement is actually ST,,  not sure what the T represents... 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    and if you want to be really sure, it should connect to the SI pin (7)  of the enc28j60 chip

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to Robert Peter Oakes

    Thx Peter.

     

    With the schematic and my multimeter i was able to confirm the pin is in fact ST..

     

    I downloaded an external library from git hub called "ethercard.h"  and my arduino is now online as a server..

    works like a charm..

     

    Funny thing though, the default Ethernet libraries don't work, and always end up with server at 0.0.0.0 error.

    While the external library works right out of the box with the included examples.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    The default libraries are for the WIZNET Ethernet chip (The one the original Arduino Ethernet Shield), not the ENC28J60 on the card you have, the newest libraries are 100% sketch code compatible but you still need to ensure you use the right one

     

    I think my tutorials lesson 4 or 5 talks about this and shows an example of using them and hosting web pages

     

    Peter