Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Infineon Shield Q/A
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 418 subscribers
  • Views 1934 views
  • Users 0 members are here
  • iot_holidaylights
Related

Infineon Shield Q/A

clem57
clem57 over 11 years ago

I would like to suggest this place for the exchange of information on this shield. I noticed a Google shows very little practical information, other than recent news announcing the shield. Since I am first, here is my question:

 

How are people going to power these and what input voltages/output voltages are expected?

 

Thanks and hoping the information share can benefit all imageimageimage

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 11 years ago in reply to alexev +1
    Thanks @ Peter Oakes and @ alexev ! I finished reading the technical details as much as I could get hands on. Seems like the shield uses I2C commands to configure many parameters from Arduino Uno master…
  • clem57
    clem57 over 11 years ago in reply to turfgnome

    True Robert,

         We all will work on project first and testing later. But here is a place to discuss/blog about experiences found I hope.

     

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gadget.iom
    gadget.iom over 11 years ago in reply to clem57

    That's an excellent point. I forgot to get some of those at the time of ordering my shield. These should do: 085 - ADAFRUIT INDUSTRIES - ARDUINO, SHIELD STACKING HEADERS | CPC

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to gadget.iom

    Also http://cpc.farnell.com/arduino/a000026/header-strip-arduino-40x1-through/dp/CN19502?crosssellid=CN19502&crosssell=true&in_merch=true& works IF you do not plan any shields above this one!

     

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to clem57

    Make sure they have really long legs or they won’t fit on the Yun, it will hit the Ethernet port before you even push it down

     

     

     

    No issues on the UNO though except you can’t stack a Ethernet shield and a RGB as there completely pin incompatible (Missing the required header pins) oh that also goes for the Yun too

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • pmohan
    pmohan over 11 years ago in reply to Robert Peter Oakes

    Cant we stack two of these together? That would resolve needing long legs?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to pmohan

    Yo can use a stacking header set to elevate the shield high enough

     

    look here

    http://www.element14.com/community/groups/arduino/blog/2014/12/16/byob-party-4-mr-uno-and-his-message-board

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to Robert Peter Oakes

    Peter,

         Was there a minimal drop on the voltage in and voltage going out? Missed the answer if you already gave this out

    Thanks,

    clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to clem57

    Hi Clem,

     

    I'm guessing you want to connect (say) an LED string designed for 12V, and power it with 12V too for example?

    If so, this will work, because the shield is designed for constant current operation, but the LED strings designed for a fixed voltage have a resistor in series to set the current level (such LED strings designed for a fixed voltage are usually controlled by just a MOSFET, and don't need a constant current circuit). In this case, the shield will adjust the voltage to the point of pushing around 300mA through the LED string, and it will reach extremely close to 12V (or whatever voltage you're using) if needed to get it to do so. If 300mA is passing through the LED string (regardless of the voltage the LED string is designed for) then it will be visibly lit (although maybe not optimally) because this is a large current, even if the voltage is lower than the 12V rating of the string.

    So, an LED string designed for 12V will become illuminated with a 12V powered shield.

    Good luck with the project!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • pmohan
    pmohan over 11 years ago

    is anyone seeing issues with color mixing? Except the primary red, green and blue, other colors don't seem to mix very well. i don't thinI its an issue with led strip itself because when I use the strip with the remote it came with, the colors look right. For example yellow. If you set red and green to equal high intensity and blue to 0, the theory is i should be seeing yellow. I see green at full intensity and the red LED at kind of half brightness. The result is a green light . Not yellow. Anyone else facing issues with color mixing ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • turfgnome
    turfgnome over 11 years ago in reply to pmohan

    I have been having the same issue I have not had a chance to go threw the code that Mr Oaks posted to try to see if my coding was wrong though.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>