Arduino Forum I need help!
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
  • Replies 11 replies
  • Subscribers 396 subscribers
  • Views 824 views
  • Users 0 members are here
Related

I need help!

matija.martinec
matija.martinec over 10 years ago

So i myself am a big arduino fanboy, I spend more than 2h a day learning something new with arduino, but how can I get others (mostly my friends) interested too.

NOTE - they mostly don't like ,as they call it "smart stuff", but if I could somehow only show them cool stuff you can do with it, but I have no idea how image.I would really like to do some kind of a club in which we could have fun and learn stuff.

 

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 10 years ago in reply to matija.martinec +4
    the only problem is that they really don't do anything else than drinking Might be time to find a new set of friends. The old saying about leading a horse to water, but you can't make them drink, applies…
  • clem57
    clem57 over 10 years ago +3
    Matija, What do your friends do? Find something they do and you can naturally incorporate the Arduino. Like a door bell that when you push plays your favorite MP on a speaker! The Arduino should be able…
  • jw0752
    jw0752 over 10 years ago +3
    Hi Matija, Another idea is to look around and see if you can find some new friends who do share your interests. I spent a lot of time trying to get my friends interested in electronics but for the most…
Parents
  • iexpress
    iexpress over 10 years ago

    Sounds awesome. When I first started programming for the AVR series MCU's, I think my first app was flashing LEDs, but then I started adding buttons so the LEDs would toggle when buttons were pressed. I think to get someone interested in electronic projects, the project would have to be something they can understand the concept of. Could be a good way to get a group together, take something you know how to do, and go over it step by step with your friends. They would probably feel proud like it was a huge accomplishment when something they built actually works, especially for the first project even if it's flashing an LED.

     

    I started programming with Atmel Studio and AVR32 MCU's like the UC3A3 series 32 bit MCU, then I switched to AVR 8-bit which is much easier.

    My last project was building a circuit board that had two ATmega328p MCU's on it controlling 4 SPI flash roms, and a bunch of digital logic.

    Then I made an ATmega programmer shield for Arduino Uno, and came up with a Visual Basic.net app to send data from HEX files to the MCU on the Arduino shield to program the AVR in the shield.

     

    Strangely, even though Arduino uses the Atmel MCU's, Atmel Studio gives you the HEX files directly, while Arduino knocks out that step and places the code onto the MCU for users, but not all the features become available when using an Arduino board. The MCU out of circuit is a bit more powerful than when on an Arduino board, but it is still very nice, especially for beginners. I think I went through all the Arduino example projects in a day or two, but I've been programming for 15 years so they seemed pretty elementary yet still fun to play around with.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed over 10 years ago in reply to iexpress

    related to Jason's comment there's the "Shrimping it" project that has some really cheap Atmel based projects to make and shows you how make an "Arduino" on a breadboard or stripboard.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Workshopshed
    Workshopshed over 10 years ago in reply to iexpress

    related to Jason's comment there's the "Shrimping it" project that has some really cheap Atmel based projects to make and shows you how make an "Arduino" on a breadboard or stripboard.