Arduino
  • Products
  • More
Arduino
Arduino Forum How to increase the range
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 416 subscribers
  • Views 429 views
  • Users 0 members are here
  • ir
  • pair
  • arduino
  • tv_remote
  • remote
Related

How to increase the range

rishi2628
rishi2628 over 11 years ago

I want to make a simple ir remote using arduino that could work within 5 meters. I tried using ir LED pair but the maximum range i got was approx 15 cm. It made me wonder that if tv remotes use the same ir LEDs and can easily work within 7 to 8 meters of range then why isn't this working ???  I am using the following 5 mm LEDs. Will please anyone suggest me how to increase the range

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +2
    LEDs used for remote are not simply turned on and off at the data rate, there also modulated with I think a 38Khz carrier in order to eliminate stray light interference etc, the receivers also have AGC…
  • gadget.iom
    gadget.iom over 11 years ago +1
    Robert Peter Oakes is absolutely right, many IR transceivers employ modulation at 38Khz to reduce interference from ambient light. The following page may be of some use: https://learn.sparkfun.com/tutorials…
Parents
  • gadget.iom
    gadget.iom over 11 years ago

    Robert Peter Oakes is absolutely right, many IR transceivers employ modulation at 38Khz to reduce interference from ambient light.

    The following page may be of some use: https://learn.sparkfun.com/tutorials/ir-control-kit-hookup-guide

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gadget.iom
    gadget.iom over 11 years ago

    Robert Peter Oakes is absolutely right, many IR transceivers employ modulation at 38Khz to reduce interference from ambient light.

    The following page may be of some use: https://learn.sparkfun.com/tutorials/ir-control-kit-hookup-guide