Arduino
  • Products
  • More
Arduino
Arduino Forum Meder Reed Switch, Digmesa Flow Meter & Arduino?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 418 subscribers
  • Views 1416 views
  • Users 0 members are here
  • sensors
  • reed
  • meter
  • flow
Related

Meder Reed Switch, Digmesa Flow Meter & Arduino?

e14 Contributor
e14 Contributor over 11 years ago

Hi,

 

Complete arduino newb and want to use this reed switch I already have MK04 Reed Sensors  It doesn't look like they make the exact model anymore (MK4-1A71-BV10102), but its a 1A/Form A with 2 wires.  Can I connect two wire sensors to Arduino or have to be 3 wires?  I think maybe I can do it this way, but don't want to fry anything.  bildr » Simple Temperature With Thermistor + Arduino  Or maybe don't connect 5v because magnet generates power?

 

Also have this flow meter http://www.digmesa.com/wp-content/uploads/2014/01/FLOW-SENSOR-FHKSC.pdf  Can I do it like this?  Seeedstudio Forum • View topic - Tutorial: Reading Water Flow rate with Water Flow Sensor  What I am not sure is the voltage, it says it is 20v or 24v.  I don't know how that affects things since Arduino 5v.

 

Thanks for any help!

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to gadget.iom +1
    I would suggest having the resistor to + 5V and the reed switch to ground, this way if the code programs the pin as an output and LOW, you’re not trying to ground the 5V rail without current limit and…
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to gadget.iom +1
    Nice find Paul Looks like you can run this in the same way as the sparkfun with only a 5V supply Peter
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago

    The reed switch is just that a switch, activated by a nearby magnet, treat it like a button on an arduino input and you should be fine as long as the wires are not too long or near hi voltage interference

     

     

     

    The thermistor / resistor pair you show in the other diagram should work by simply feeding the junction of the two into the analog input of the Arduino, A5 for instance

     

     

     

    The reed switch is not a magnet and has no coils to generate power, it is simply a switch contact that closes when a magnetic field is close enough to make the contacts pull together (Or separate depending on the model)

     

     

     

    The flow sensor has two issues,

     

    1.       It runs on 20 or 24V or so it seems, you most lightly won’t have this available to you easily without buying an adapter

     

    2.       It does not specify the output pulse, this could be a relay contact closure, a hall effect sensor or something completely different so until you know it is tough to advise, I suggest hooking it up to a meter (Not Arduino) and powering it up to see what it gives out, if you can find more product details that would help us advise you

     

    Technically you can do something similar to the example linked in but your interface would be different depending on the output and actual supply of the flow meter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago

    The reed switch is just that a switch, activated by a nearby magnet, treat it like a button on an arduino input and you should be fine as long as the wires are not too long or near hi voltage interference

     

     

     

    The thermistor / resistor pair you show in the other diagram should work by simply feeding the junction of the two into the analog input of the Arduino, A5 for instance

     

     

     

    The reed switch is not a magnet and has no coils to generate power, it is simply a switch contact that closes when a magnetic field is close enough to make the contacts pull together (Or separate depending on the model)

     

     

     

    The flow sensor has two issues,

     

    1.       It runs on 20 or 24V or so it seems, you most lightly won’t have this available to you easily without buying an adapter

     

    2.       It does not specify the output pulse, this could be a relay contact closure, a hall effect sensor or something completely different so until you know it is tough to advise, I suggest hooking it up to a meter (Not Arduino) and powering it up to see what it gives out, if you can find more product details that would help us advise you

     

    Technically you can do something similar to the example linked in but your interface would be different depending on the output and actual supply of the flow meter