Arduino
  • Products
  • More
Arduino
Arduino Forum Meder Reed Switch, Digmesa Flow Meter & Arduino?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 418 subscribers
  • Views 1419 views
  • Users 0 members are here
  • sensors
  • reed
  • meter
  • flow
Related

Meder Reed Switch, Digmesa Flow Meter & Arduino?

e14 Contributor
e14 Contributor over 11 years ago

Hi,

 

Complete arduino newb and want to use this reed switch I already have MK04 Reed Sensors  It doesn't look like they make the exact model anymore (MK4-1A71-BV10102), but its a 1A/Form A with 2 wires.  Can I connect two wire sensors to Arduino or have to be 3 wires?  I think maybe I can do it this way, but don't want to fry anything.  bildr » Simple Temperature With Thermistor + Arduino  Or maybe don't connect 5v because magnet generates power?

 

Also have this flow meter http://www.digmesa.com/wp-content/uploads/2014/01/FLOW-SENSOR-FHKSC.pdf  Can I do it like this?  Seeedstudio Forum • View topic - Tutorial: Reading Water Flow rate with Water Flow Sensor  What I am not sure is the voltage, it says it is 20v or 24v.  I don't know how that affects things since Arduino 5v.

 

Thanks for any help!

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to gadget.iom +1
    I would suggest having the resistor to + 5V and the reed switch to ground, this way if the code programs the pin as an output and LOW, you’re not trying to ground the 5V rail without current limit and…
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to gadget.iom +1
    Nice find Paul Looks like you can run this in the same way as the sparkfun with only a 5V supply Peter
Parents
  • dmaruska
    dmaruska over 11 years ago

    Without looking at the datasheet, the reed switches will come in different forms.  Normally Closed (NC) or Normally Open (NO), or a Com and both NO and NC.  So depending on the one you are using, you will want to use either a pull up resistor or pull down.  Depending on how you hook the wires, to +5vdc or GND, if you connect one side to +5vdc on the NO side of the switch, used a pull down on the other side to a Digital Pin in.  This will keep the Digital pin from floating and can give you a wrong indication.  You will have to play with the NO or NC type of switch for best results.  The Magnet will wither open or close the Reed switch depending on what you are using.  This will hold true for any type of switched input.  Your pull up or pull down can be 10K ohm for larger.  Play with it until you have the best results.

     

    Regards,

     

    Dave M.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dmaruska
    dmaruska over 11 years ago

    Without looking at the datasheet, the reed switches will come in different forms.  Normally Closed (NC) or Normally Open (NO), or a Com and both NO and NC.  So depending on the one you are using, you will want to use either a pull up resistor or pull down.  Depending on how you hook the wires, to +5vdc or GND, if you connect one side to +5vdc on the NO side of the switch, used a pull down on the other side to a Digital Pin in.  This will keep the Digital pin from floating and can give you a wrong indication.  You will have to play with the NO or NC type of switch for best results.  The Magnet will wither open or close the Reed switch depending on what you are using.  This will hold true for any type of switched input.  Your pull up or pull down can be 10K ohm for larger.  Play with it until you have the best results.

     

    Regards,

     

    Dave M.