Arduino
  • Products
  • More
Arduino
Arduino Forum Meder Reed Switch, Digmesa Flow Meter & Arduino?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 418 subscribers
  • Views 1418 views
  • Users 0 members are here
  • sensors
  • reed
  • meter
  • flow
Related

Meder Reed Switch, Digmesa Flow Meter & Arduino?

e14 Contributor
e14 Contributor over 11 years ago

Hi,

 

Complete arduino newb and want to use this reed switch I already have MK04 Reed Sensors  It doesn't look like they make the exact model anymore (MK4-1A71-BV10102), but its a 1A/Form A with 2 wires.  Can I connect two wire sensors to Arduino or have to be 3 wires?  I think maybe I can do it this way, but don't want to fry anything.  bildr » Simple Temperature With Thermistor + Arduino  Or maybe don't connect 5v because magnet generates power?

 

Also have this flow meter http://www.digmesa.com/wp-content/uploads/2014/01/FLOW-SENSOR-FHKSC.pdf  Can I do it like this?  Seeedstudio Forum • View topic - Tutorial: Reading Water Flow rate with Water Flow Sensor  What I am not sure is the voltage, it says it is 20v or 24v.  I don't know how that affects things since Arduino 5v.

 

Thanks for any help!

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to gadget.iom +1
    I would suggest having the resistor to + 5V and the reed switch to ground, this way if the code programs the pin as an output and LOW, you’re not trying to ground the 5V rail without current limit and…
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to gadget.iom +1
    Nice find Paul Looks like you can run this in the same way as the sparkfun with only a 5V supply Peter
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    Wow! Thanks for all the replies, I think I can work through it.  Gotta order the arduino, but waiting until I knew if I could use what I already had.  May have some more questions down the road, but thanks a bunch you guys, I really appreciate it.  It's for espresso machine I am building here if you want to check it out...Homeroasters.org - Discussion Forum: Starbucks (Saeco) Sirena

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 11 years ago

    Wow! Thanks for all the replies, I think I can work through it.  Gotta order the arduino, but waiting until I knew if I could use what I already had.  May have some more questions down the road, but thanks a bunch you guys, I really appreciate it.  It's for espresso machine I am building here if you want to check it out...Homeroasters.org - Discussion Forum: Starbucks (Saeco) Sirena