Arduino Forum Could I just push these pins into a breadboard?
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
  • Replies 4 replies
  • Subscribers 403 subscribers
  • Views 549 views
  • Users 0 members are here
  • wifi
  • pins
  • transceiver
  • breadboard
  • arduino
Related

Could I just push these pins into a breadboard?

Former Member
Former Member over 10 years ago

ESP8266 ESP-01 Remote Serial Port WIFI Transceiver Wireless Module Sale-Banggood.com

 

I was looking at this lovely wifi serial transceiver module when I looked at the picture of the pins. There are 8 pins but they are in rows of 4. The seems pretty strange and I couldn't just put it into a breadboard could I? If I couldn't would I have to solder wires onto the pins and hook it up that way? I would really prefer not to go there. Anyways I would love the help. Thank you in advance. image

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +1
    cant just plug into the bread board as there is no where to separate the two rows, there too close together what I do is use a female to female jumper leads and push header pins into the breadboard to…
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    cant just plug into the bread board as there is no where to separate the two rows, there too close together

     

    what I do is use a female to female jumper leads and push header pins into the breadboard to connect that end, works well for me

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    cant just plug into the bread board as there is no where to separate the two rows, there too close together

     

    what I do is use a female to female jumper leads and push header pins into the breadboard to connect that end, works well for me

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mcb1
    mcb1 over 10 years ago in reply to Robert Peter Oakes

    jacob_pickens

    Robert Peter Oakes

     

    But you could with these.

    http://www.banggood.com/ESP8266-ESP-07-Remote-Serial-Port-WIFI-Transceiver-Wireless-Module-p-961247.html

    http://www.banggood.com/ESP8266-ESP-11-Remote-Serial-Port-WIFI-Transceiver-Wireless-Module-p-961251.html

     

    Mark