Arduino
  • Products
  • More
Arduino
Arduino Forum Multiple signals to same pcb?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 418 subscribers
  • Views 976 views
  • Users 0 members are here
Related

Multiple signals to same pcb?

e14 Contributor
e14 Contributor over 11 years ago

Hi, so I have little pcb with 2 leds and 2 switches on it.  A common wire goes to one side of all of 4 items and a single wire goes to other side of each item, for a total of 5 wires.  In addition, there is what looks like a resistor connecting both sides of the leds.  My issue is that to get an led to light up, I have to connect the common wire to the signal of pin 12, for example, and the individual wire for that led to ground.

 

This is causing great confusion and pain and suffering on my end.  I presume that I can not connect the signal of 4 different arduino pins to the common wire on the pcb without doing something else, if at all?  I can connect the switches normally, but I presume using the same connection as both signal for the switches and ground for the leds will also not be a good idea.  Anyway, board designed and engineered precisely and replicating with different wiring would be very difficult for me.  Thanks for any advice!

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +1
    you may have something like this (Based on description) hope this helps did you make the board yourself and are having difficulty getting it to work or is it a bought product? can you provide a picture…
Parents
  • 4ringfan
    4ringfan over 11 years ago

    Joe,

     

    Is your intent to push button #1 and have LED #1 light up, and/or press button #2 and have LED #2 light up?  What exactly are you trying to accomplish?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to 4ringfan

    If I connect the common wire to 4 different arduino pin signal wires, then is that problem? Reason being they may be active at the same time, so having two signal wires connected to the same circuit and each signaling at same maybe time burn something out?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to 4ringfan

    If I connect the common wire to 4 different arduino pin signal wires, then is that problem? Reason being they may be active at the same time, so having two signal wires connected to the same circuit and each signaling at same maybe time burn something out?