Arduino
  • Products
  • More
Arduino
Arduino Forum Multiple signals to same pcb?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 418 subscribers
  • Views 975 views
  • Users 0 members are here
Related

Multiple signals to same pcb?

e14 Contributor
e14 Contributor over 11 years ago

Hi, so I have little pcb with 2 leds and 2 switches on it.  A common wire goes to one side of all of 4 items and a single wire goes to other side of each item, for a total of 5 wires.  In addition, there is what looks like a resistor connecting both sides of the leds.  My issue is that to get an led to light up, I have to connect the common wire to the signal of pin 12, for example, and the individual wire for that led to ground.

 

This is causing great confusion and pain and suffering on my end.  I presume that I can not connect the signal of 4 different arduino pins to the common wire on the pcb without doing something else, if at all?  I can connect the switches normally, but I presume using the same connection as both signal for the switches and ground for the leds will also not be a good idea.  Anyway, board designed and engineered precisely and replicating with different wiring would be very difficult for me.  Thanks for any advice!

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +1
    you may have something like this (Based on description) hope this helps did you make the board yourself and are having difficulty getting it to work or is it a bought product? can you provide a picture…
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    Here is the board.

     

    image

     

    But I am looking at Mike's led pic and thinking maybe I didn't understand how leds work, which is to say that full current doesn't flow through the led, if at all, but current flows more around the led so to speak and stuff happens between the two sides and the resistor limits the current going around the two sides so not too much stuff happens between the two sides or poof?  So they are resistors and they aren't in parallel, they just look like they are.

     

    So getting back to my original question, thinking now even if bad stuff doesn't happen between the arduino pins, it's moot because both leds would light up on either signal because arduino has individual positive and common ground, whereas the proprietary computer this board was connected to clearly has individual ground and common positive.  That means I either have to turn the led's around to change the common to ground or cut this thing and add more wires.

     

    Anyway, anyone feel free to correct me if any of that sounds wrong.  Also any ideas are welcome.

     

    Thanks again for all your help!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 11 years ago

    Here is the board.

     

    image

     

    But I am looking at Mike's led pic and thinking maybe I didn't understand how leds work, which is to say that full current doesn't flow through the led, if at all, but current flows more around the led so to speak and stuff happens between the two sides and the resistor limits the current going around the two sides so not too much stuff happens between the two sides or poof?  So they are resistors and they aren't in parallel, they just look like they are.

     

    So getting back to my original question, thinking now even if bad stuff doesn't happen between the arduino pins, it's moot because both leds would light up on either signal because arduino has individual positive and common ground, whereas the proprietary computer this board was connected to clearly has individual ground and common positive.  That means I either have to turn the led's around to change the common to ground or cut this thing and add more wires.

     

    Anyway, anyone feel free to correct me if any of that sounds wrong.  Also any ideas are welcome.

     

    Thanks again for all your help!